ZHCSKV6B March 2020 – February 2024 TPA6211T-Q1
PRODUCTION DATA
Place all the external components close to the TPA6211T-Q1 device. The input resistors need to be close to the device input pins so noise does not couple on the high impedance nodes between the input resistors and the input amplifier of the device. Placing the decoupling capacitors, CS and CBYPASS, close to the TPA6211T-Q1 device is important for the efficiency of the amplifier. Any resistance or inductance in the trace between the device and the capacitor can cause a loss in efficiency.