ZHCSMU9A December 2020 – September 2021 TAS2764
PRODUCTION DATA
The TAS2764 provides a flexible TDM serial audio port. The port can be configured to support a variety of formats including stereo I2S, Left Justified and TDM. Mono audio playback is available via the SDIN pin. The SDOUT pin is used to transmit sample streams including speaker voltage and current sense, PVDD voltage, die temperature and channel gain.
The TDM serial audio port supports up to 16 of 32-bit time slots at 44.1/48 kHz or 8 of 32-bit time slots at a 88.2/96 kHz sample rate. Valid SBCLK to FSYNC ratios are 16, 24, 32, 48, 64, 96, 128, 192, 256, and 512. The device will automatically detect the number of time slots and it does not need to be programmed.
By default, the TAS2764 will automatically detect the PCM playback sample rate. This can be disabled and manually configured by setting the AUTO_RATE register bit high.
The SAMP_RATE[2:0] and SAMP_RATIO[3:0] register bits are used to configure the PCM audio sample rate when AUTO_RATE register bit is high (auto detection of TDM sample rate is disabled). The TAS2764 employs a robust clock fault detection engine that will automatically volume ramp down the playback path if FSYNC does not match the configured sample rate (if AUTO_RATE = 1) or the ratio of SBCLK to FSYNC is not supported (minimizing any audible artifacts). Once the clocks are detected to be valid in both frequency and ratio, the device will automatically volume ramp the playback path back to the configured volume and resume playback.
When using the auto rate detection the sampling rate and SBCLK to FSYNC ration detected on the TDM bus is reported back on the read-only register bits FS_RATE[2:0] and FS_RATIO[3:0] respectively.
The TAS2764 supports a 12 MHz SBCLK operation. The system will detect or should be manually configured for a ratio of 125 or 250. In this specific ratio the last 32-bit slot should not be used to transmit data over the TDM port (Section 8.4.1) or ICC pin ( Section 8.4.2.9.1) as data will be truncated.
Figure 8-2 and Figure 8-3 below illustrate the receiver frame parameters required to configure the port for playback. A frame begins with the transition of FSYNC from either high to low or low to high (set by the FRAME_START register bit). FSYNC and SDIN are sampled by SBCLK using either the rising or falling edge (set by the RX_EDGE register bit). The RX_OFFSET[4:0] register bits define the number of SBCLK cycles from the transition of FSYNC until the beginning of time slot 0. This is typically set to a value of 0 for Left Justified format and 1 for an I2S format.
The RX_SLEN[1:0] register bits set the length of the RX time slot to 16, 24 or 32 (default) bits. The length of the audio sample word within the time slot is configured by the RX_WLEN[1:0] register bits to 16, 20, 24 (default) or 32 bits. The RX port will left justify the audio sample within the time slot by default, but this can be changed to right justification via the RX_JUSTIFY register bit. The TAS2764 supports mono and stereo down mix playback ([L+R]/2). By default the device will playback mono from the time slot equal to the I2C base address offset (set by the ADDR pin) for playback. The RX_SCFG[1:0] register bits can be used to override the playback source to the left time slot, right time slot or stereo down mix set by the RX_SLOT_L[3:0] and RX_SLOT_R[3:0] register bits.
If time slot selection places reception either partially or fully beyond the frame boundary, the receiver will return a null sample equivalent to a digitally muted sample.
The TDM port can transmit a number of sample streams on the SDOUT pin including speaker voltage sense, speaker current sense, interrupts and status, PVDD voltage, die temperature and channel gain. Figure 8-4 below illustrates the alignment of time slots to the beginning of a frame and how a given sample stream is mapped to time slots.
Either the rising or falling edge of SBCLK can be used to transmit data on the SDOUT pin. This can be configured by setting the TX_EDGE register bit. The TX_OFFSET[2:0] register bits define the number SBCLK cycles between the start of a frame and the beginning of time slot 0. This would typically be programmed to 0 for Left Justified format and 1 for I2S format. The TDM and ICC TX can either transmit logic 0 or Hi-Z depending on the setting of the TX_FILL register bit. An optional bus keeper will weakly hold the state of SDOUT and ICC pins when all devices driving are Hi-Z. Since only one bus keeper is required on SDOUT, this feature can be disabled via the TX_KEEPEN register bit. The bus keeper can be configured to hold only 1LSB or Always using TX_KEEPLN register bit. Additionally, the keeper LSB can be driven for a full cycle or half of cycle using TX_KEEPCY register bit.
TX_FILL is used in mono system where there is only one amplifier on I2S bus. All the slots unused by the amplifier will be filled with zeros when TX_FILL is set to low.
The SDOUT_HIZ registers from page 0x01 are useful when multiple devices are on the same I2S bus. Each device does not know configuration of slots in the other devices on the bus. It is required at the system level to program the SDOUT_HIZ registers appropriately, in such way that the settings are done correctly and do not create any contention both internally and externally.
Each sample stream is composed of either one or two 8-bit time slots. Speaker voltage sense and speaker current sense sample streams are 16-bit precision, so they will always utilize two TX time slots. The PVDD voltage stream is 12 bit precision, and can either be transmitted left justified in a 16-bit word (using two time slots) or can be truncated to 8-bits (the top 8 MSBs) and be transmitted in a single time slot. This is configured by setting PVDD_SLEN register bit. The Die temperature and gain are both 8-bit precision and are transmitted in a single time slot.
The time slot register for each sample stream defines where the MSB transmission begins. For instance, if VSNS_SLOT[5:0] register bits are set to 2 (decimal), the upper 8 MSBs will be transmitted in time slot 2 and the lower 8 LSBs will be transmitted in time slot 3. Each sample stream can be individually enabled or disabled by using VSNS_TX and ISNS_TX register bits. This is useful to manage limited TDM bandwidth since it may not be necessary to transmit all streams for all devices on the bus.
It is important to ensure that time slot assignments for actively transmitted sample streams do not conflict. For instance, if VSNS_SLOT[5:0] bits are set to 2 (decimal) and ISNS_SLOT[5:0] bits are set to 3 (decimal), the lower 8 LSBs of voltage sense will conflict with the upper 8 MSBs of current sense. This will produce unpredictable transmission results in the conflicting bit slots (i.e. the priority is not defined).
When two or more devices are connected to the same SDOUT pin the slot assignment of the various devices must be kept exclusive to avoid any contention. This constraint is applicable to both Software Shutdown and Active Mode. Devices should not be programmed to transmit on the same slot.
The current and voltage values are transmitted at the full 16-bit measured values by default. The IVMON_LEN[1:0] register bits can be used to transmit only the 8 MSB bits in one slot or 12 MSB bits values across multiple slots. The special 12-bit mode is used when only 24-bit I2S/TDM data can be processed by the host processor. The device should be configured with the voltage-sense slot and current-sense slot off by 1 slot and will consume 3 consecutive 8-bit slots. In this mode the device will transmit the first 12 MSB bits followed by the second 12 MSB bits specified by the preceding slot.
If time slot selections place transmission beyond the frame boundary, the transmitter will truncate transmission at the frame boundary.
The time slots for VBAT1S, PVDD and TEMP measurements are set using VBAT1S_SLOT[5:0], PVDD_SLOT[5:0] and TEMP_SLOT[5:0] register bits. To enable sample stream register bits VBAT1S_TX, PVDD_TX and TEMP_TX must be set high. The slot length is selected by VBAT1S_SLEN, PVDD_SLEN and TEMP_SLEN register bits.
To set TDM final processed audio slot, enable and length register bits the following register bits need to be programmed: AUDIO_SLOT[5:0], AUDIO_TX and AUDIO_SLEN .
Information about status of slots can be find in STATUS_SLOT[5:0] register bits. STATUS_TX register bit set high enables the status transmit.
The slot configuration for the TX limiter gain reduction can be set between 0 (default) and 63 by setting GAIN_SLOT[5:0] register bits. It is used for the Inter Chip Gain Aligment ( Section 8.4.2.9 ) and can be either over the TDM Bus or ICC pin (Section 8.4.2.9.1). To use this feature, the register bit GAIN_TX needs to be set high (Enable).