ZHCSPB0 april 2023 LM5171-Q1
ADVANCE INFORMATION
The LM5171-Q1 also integrates two Op-Amps serving as the outer voltage loop error amplifiers, one for the buck mode operation, the other for the boost mode operation. For the channel independent operation, these two Op-Amps can be used for CH-1, and the users need to use two external Op-Amps for CH-2. Once the inner current loop is closed, the outer voltage loop is also a first order system and a Type-II compensation network can be used to stabilize the LM5171-Q1 output voltage loop. Refer to the Section 8.1 section for details of the compensation network selection criteria.