ZHCSPB0 april 2023 LM5171-Q1
ADVANCE INFORMATION
When the current loop compensator is designed, the outer voltage loop can then be analyzed. Figure 8-4 shows the outer voltage control loop and inner current loop.
We can get the close loop transfer function from ISET to the output voltage (vO) as:
When selecting the crossover frequency of the buck voltage loop lower than the current loop crossover frequency, Gvs(s) can be simplified. For the denominator, Ti(s) dominates, Equation 49 can be written as:
The buck power plant transfer function from the duty cycle (d) to the output voltage (vLV) is determined by the following:
where
Substituting Equation 51 into Equation 50, a simplified transfer function from the ISET voltage to the Output voltage (VLV) is determined by the following:
where
Similarly, the boost power plant transfer function from the duty cycle (d) to the output voltage (vHV) is determined by the following:
where
Substituting Equation 55 into Equation 50, a simplified transfer function from the ISET voltage to the output voltage (VHV) is determined by the following:
where