ZHCSPB0 april 2023 LM5171-Q1
ADVANCE INFORMATION
TI recommends setting a hard limit of the maximum current programming signal such that the converter cannot be over driven by an errant current programming signal. Assume the converter is allowed up to 10% overloading current. Refer to Channel Current Setting Commands (ISET1 and ISET2), the analog current setting signal ISETx must be limited by the following voltage level:
As shown in Figure 8-5, RISETT and RISETB are used to limit the maximum voltage on ISETx.