ZHCSG37C September 2016 – December 2022 DS90UB934-Q1
PRODUCTION DATA
The DS90UB934-Q1 has two input ports that operate as a multiplexer controlled by the SEL pin. A single camera can be connected to either Rx input port 0 or Rx input port 1 (Figure 6-9).
Two cameras can be connected simultaneously, but only one is active at a time (Figure 6-10). The SEL pin can be toggled on-the-fly to select which camera is forwarded to the DVP output.
Figure 6-9 DS90UB933-Q1 Camera Data to 1 Rx Port
Figure 6-10 Two DS90UB933-Q1 Camera Data to 2 Rx Ports