ZHCSIA7 May 2018 DLPA4000
PRODUCTION DATA.
The DLPA4000 contains three general purpose buck converters and a supporting LDO (LDO_BUCKS). The three programmable 8-bit buck converters generate a voltage between 1 V and 5 V. The buck converters have an output current limit of 2 A. The device supports only General Purpose Buck2 (PWR6) types. Figure 16 shows one of the buck converters and the LDO_BUCKS.
The two DMD or DLPC buck converters discussed earlier in DMD Supplies have the same architecture as these three buck converters and can be configured in the same way.
Figure 16. Buck Converter