SWRS045F January 2006 – November 2018 CC1021
PRODUCTION DATA.
TI provides users of the CC1021 device with a software program, SmartRF™ Studio (Windows interface), that generates all necessary CC1021 device configuration data based on the user's selections of various parameters. These hexadecimal numbers will then be the necessary input to the microcontroller for the configuration of the CC1021 device. In addition, the program will provide the user with the component values needed for the input/output matching circuit, the PLL loop filter and the LC filter.
Figure 5-2 shows the user interface of the CC1021 device configuration software.
Figure 5-2 SmartRF™ Studio User Interface