ZHCU578 October 2018
The rectifier diode (D1) must also stand off the input voltage plus the output voltage and be rated for the maximum output current. These ratings can be calculated using the following equations:
A 100-V, 8-A Q-grade schottky diode is chosen for D1.