SLUSAM9E July 2011 – April 2020
PRODUCTION DATA.
The BQ76925 device integrates cell-balancing FETs that are individually controlled by the Host. The balancing method is resistive bleed balancing, where the balancing current is set by the external cell input resistors. The maximum allowed balancing current is 50 mA per cell.
The Host may activate one or more cell balancing FETs by writing the BAL_n bits in the BAL_CTL register. To allow the greatest flexibility, the Host has complete control over the balancing FETs. However, in order to avoid exceeding the maximum cell input voltage, the BQ76925 will prevent two adjacent balancing FETs from being turned on simultaneously. If two adjacent bits in the balance control register are set to 1, neither balancing transistor will be turned on. The Host based balancing algorithm must also limit the power dissipation to the maximum ratings of the device.
In a normal system, closing a cell-balancing FET will cause 2 cell voltages to appear across one cell input. This fact can be utilized to detect a cell sense-line open condition, that is, a broken wire from the cell-sense point to the BQ76925 VCn input. Table 3 shows how this can be accomplished. Note that the normal cell-voltage measurements may represent a saturated or full-scale reading. However, these will normally be distinguishable from the open-cell measurement.
Kelvin input to test | Method 1 | Method 2 | ||||||
---|---|---|---|---|---|---|---|---|
Turn On | Measure | Result | Turn On | Measure | Result | |||
Normal | Open | Normal | Open | |||||
VC0 | BAL_1 | CELL2 | CELL2 + 0.5 × CELL1 | CELL2 | ||||
VC1 | BAL_2 | CELL3 | CELL3 + 0.5 × CELL2 | CELL3 | ||||
VC2 | BAL_3 | CELL4 | CELL4 + 0.5 × CELL3 | CELL4 | BAL_2 | CELL1 | CELL1 + 0.5 × CELL2 | CELL1 |
VC3 | BAL_4 | CELL5 | CELL5 + 0.5 × CELL4 | CELL5 | BAL_3 | CELL2 | CELL2 + 0.5 × CELL3 | CELL2 |
VC4 | BAL_5 | CELL6 | CELL6 + 0.5 × CELL5 | CELL6 | BAL_4 | CELL3 | CELL3 + 0.5 × CELL4 | CELL3 |
VC5 | BAL_5 | CELL4 | CELL4 + 0.5 × CELL5 | CELL4 | ||||
VC6 | BAL_6 | CELL5 | CELL5 + 0.5 × CELL6 | CELL5 |
NOTE
The cell amplifier headroom limits discussed above apply to the open-cell detection method because by virtue of closing a switch between 2 cell inputs, internal to the device this appears as an extreme cell imbalance. Therefore, when testing for an open on CELL2 by closing the CELL1 balancing FET, the CELL2 measurement will be less than the expected normal result due to gain loss caused by the imbalance. However, the CELL2 measurement will still increase under this condition so that a difference between open (no change) and normal (measured voltage increases) can be detected.