SLUSAM9E July 2011 – April 2020
PRODUCTION DATA.
The Host reads from the registers of the BQ76925 device as shown in Figure 14. This protocol is similar to the write protocol, except that the slave now drives data back to the Host. The BQ76925 device acknowledges each received byte by pulling the SDA line low during the acknowledge period. When the BQ76925 device sends data back to the Host, the Host drives the acknowledge.
The Host may optionally request a CRC byte following the Data byte as shown. The CRC for read commands is always enabled, but not required. If the CRC is not used, then the Host simply NACK’s the Data byte and then generates the Stop condition.