ZHCSSM4E August 1999 – March 2024 TPS766
PRODUCTION DATA
The enable pin for the device is an active-low pin. The output voltage is enabled when the voltage of the enable pin is lower than the low-level input voltage of the EN pin, and is disabled when the enable pin voltage is higher than the high-level input voltage of the EN pin. If EN functionality is not needed, connect the enable pin to the GND of the device.
For the new chip, there is an internal pullup current on the EN pin. Therefore, leave the EN pin floating. If the EN pin is left floating, the LDO is disabled.
In the new chip, the device has an internal output pulldown circuit that activates when the device is disabled to actively discharge the output voltage; see the Output Pulldown section.