ZHCSKI6T January 2006 – December 2023 TPS737
PRODUCTION DATA
请参考 PDF 数据表获取器件具体的封装图。
Using the thermal metrics ΨJT and ΨJB, as shown in the Thermal Information table, the junction temperature can be estimated with corresponding formulas (given in Equation 8). For backward compatibility, an older θJC,Top parameter is listed as well.
where:
For more information about measuring TT and TB, see the Using New Thermal Metrics application note, available for download at www.ti.com.
As Figure 7-7 shows, the new thermal metrics (ΨJT and ΨJB) have very little dependency on board size. That is, using ΨJT or ΨJB with Equation 8 is a good way to estimate TJ by simply measuring TT or TB, regardless of the application board size.
For a more detailed discussion of why TI does not recommend using θJC(top) to determine thermal characteristics, see the Using New Thermal Metrics application note, available for download at www.ti.com. For further information, see the Semiconductor and IC Package Thermal Metrics application note, also available on the TI website. Figure 7-8 shows the measuring points for DRB, DRV, and DCQ packages.