ZHCS089G February 2011 – September 2017 TPS65185
PRODUCTION DATA.
The device is designed to operate with an input voltage supply range from 3 V to 6 V, where Figure 5 and Figure 6 show how lower input supply voltages can result in larger inrush currents. This input supply can be from a externally regulated supply. If the input supply is located more than a few inches from the TPS65185x, additional bulk capacitance may be required in addition to the ceramic bypass capacitors. An electrolytic capacitor with a value of 10 µF is a typical choice.