ZHCSFJ2C September 2015 – February 2019 TPS65094
PRODUCTION DATA.
For a detailed description regarding layout recommendations, refer to the TPS65094x Design Guide and to the TPS65094x Schematic Checklist, Layout Checklist, and ILIM Calculator Tool. For all switching power supplies, the layout is an important step in the design, especially at high peak currents and high switching frequencies. If the layout is not carefully done, the regulator can have stability problems and EMI issues. Therefore, use wide and short traces for the main current path and for the power ground tracks. The input capacitors, output capacitors, and inductors must be placed as close as possible to the device. Use a common-ground node for power ground and use a different, isolated node for control ground to minimize the effects of ground noise. Connect these ground nodes close to the AGND pin by one or two vias. Use of the design guide is highly encouraged in addition to the following list of other basic requirements: