ZHCSIZ1G May 2010 – November 2018 LM98640QML-SP
PRODUCTION DATA.
To write to the serial registers using the four wire interface, the timing diagram shown in Figure 26 must be met. First, SEN is toggled low. At the rising edge of the first clock, the master should assume control of the SDI pin and begin issuing the write command. The write command is built of a "write" bit (0), device address bit (0), six bit register address, and eight bit register value to be written. SDI is clocked into the LM98640QML-SP at the rising edge of SCLK. The LM98640QML-SP assumes control of the SDO pin during the first eight clocks of the cycle. During this period, data is clocked out of the device at the rising edge of SCLK. The eight bit value clocked out is the contents of the previously addressed register, regardless if the previous command was a read or a write. When SEN toggles high, the register is written to, and the LM98640QML-SP now functions with this new data.