ZHCSKH7 November 2019 LDC1001
PRODUCTION DATA.
Use Equation 10 to calculate the minimum sensor frequency.
In Equation 10, M is 218.96, which rounds to 219 decimal. This value should to be written into Watchdog Timer Register (address 0x03).
The LDC1001 includes a watchdog which monitors the sensor oscillation and flags an error in the STATUS register if no transitions occur on the sensor in a given time window. The time window is controlled by the Min Frequency setting. If the Min Sensor Frequency is programmed for too high a frequency, the watchdog will erroneously indicate that the sensor has stopped oscillating. If the Min Sensor Frequency is set too low, then the LDC1001 will take a longer time to detect if the sensor oscillation has stopped.