ZHCSKH7 November 2019 LDC1001
PRODUCTION DATA.
Following the steps listed in the Choosing Filter Capacitor (CFA and CFB Pins) section, the filter capacitor for the example sensor is 20 pF. Figure 18 and Figure 19 show the pattern on CFB pin with a 100-pF and 20-pF filter capacitor. Notice that the timescale of scope traces is sufficient to vew the waveform over many cycles of the sensor oscillation.