ZHCSJU7 May 2019 DRV8340-Q1
PRODUCTION DATA.
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | CPL | PWR | Charge pump switching node. Connect a flying capacitor between the CPH and CPL pins |
2 | CPH | PWR | Charge pump switching node. Connect a flying capacitor between the CPH and CPL pins |
3 | VCP | PWR | Charge pump output. Connect a bypass capacitor between the VCP and VM pins |
4 | VM | PWR | Gate driver power supply input. Connect to the bridge power supply. Connect bypass capacitors VM and PGND pins |
5 | VDRAIN | I | High-side MOSFET drain sense input. Connect to the common point of the MOSFET drains |
6 | GHA | O | High-side gate driver output. Connect to the gate of the high-side power MOSFET |
7 | SHA | I | High-side source sense input. Connect to the high-side power MOSFET source. If high-side power MOSFET is not used, connect to GND |
8 | DLA | I | Low-side MOSFET drain sense input. Connect to the low-side MOSFET drain |
9 | GLA | O | Low-side gate driver output. Connect to the gate of the low-side power MOSFET |
10 | SLA | I | Low-side source sense input. Connect to the low-side power MOSFET source |
11 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
12 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
13 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
14 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
15 | SLB | I | Low-side source sense input. Connect to the low-side power MOSFET source |
16 | GLB | O | Low-side gate driver output. Connect to the gate of the low-side power MOSFET |
17 | DLB | I | Low-side MOSFET drain sense input. Connect to the low-side MOSFET drain |
18 | SHB | I | High-side source sense input. Connect to the high-side power MOSFET source. If high-side power MOSFET is not used, connect to GND |
19 | GHB | O | High-side gate driver output. Connect to the gate of the high-side power MOSFET |
20 | GHC | O | High-side gate driver output. Connect to the gate of the high-side power MOSFET |
21 | SHC | I | High-side source sense input. Connect to the high-side power MOSFET source. If high-side power MOSFET is not used, connect to GND |
22 | DLC | I | Low-side MOSFET drain sense input. Connect to the low-side MOSFET drain |
23 | GLC | O | Low-side gate driver output. Connect to the gate of the low-side power MOSFET |
24 | SLC | I | Low-side source sense input. Connect to the low-side power MOSFET source |
25 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
26 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
27 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
28 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
29 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
30 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
31 | nFAULT | OD | Fault indicator output. This pin is pulled logic low during a fault condition and requires an external pullup resistor |
32 | MODE | I | PWM input mode setting. This pin is a 7-level input pin set by an external resistor |
33 | IDRIVE | I | Gate drive output current setting. This pin is a 7-level input pin set by an external resistor |
34 | VDS | I | VDS monitor trip point setting. This pin is a 7-level input pin set by an external resistor |
35 | RSVD | I | Reserved. Leave open. |
36 | ENABLE | I | Gate driver enable. When this pin is logic low the device goes to a low-power sleep mode. An 20-μs (typ) low pulse can be used to reset fault conditions |
37 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
38 | AGND | PWR | Device analog ground. Connect to system ground |
39 | DVDD | PWR | 3.3-V internal regulator output. Connect a bypass capacitor between the DVDD and AGND pins. This regulator can externally source up to 30 mA. |
40 | nDIAG | I | Control pin for open load diagnostic and offline short-to-battery and short-to-ground diagnostic. To enable the diagnostics at device power-up, do not connect this pin (or tie it to ground). To disable the diagnostics, connect this pin to the DVDD pin. |
41 | INHA | I | High-side gate driver control input. This pin controls the output of the high-side gate driver |
42 | INLA | I | Low-side gate driver control input. This pin controls the output of the low-side gate driver |
43 | INHB | I | High-side gate driver control input. This pin controls the output of the high-side gate driver |
44 | INLB | I | Low-side gate driver control input. This pin controls the output of the low-side gate driver |
45 | INHC | I | High-side gate driver control input. This pin controls the output of the high-side gate driver |
46 | INLC | I | Low-side gate driver control input. This pin controls the output of the low-side gate driver |
47 | PGND | PWR | Device power ground. Connect to system ground |
48 | NC | NC | No connect. Do not connect anything to this pin |
— | Thermal Pad | PWR | Must be connected to ground |
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | CPL | PWR | Charge pump switching node. Connect a flying capacitor between the CPH and CPL pins |
2 | CPH | PWR | Charge pump switching node. Connect a flying capacitor between the CPH and CPL pins |
3 | VCP | PWR | Charge pump output. Connect a bypass capacitor between the VCP and VM pins |
4 | VM | PWR | Gate driver power supply input. Connect to the bridge power supply. Connect bypass capacitors between the VM and PGND pins |
5 | VDRAIN | I | High-side MOSFET drain sense input. Connect to the common point of the MOSFET drains |
6 | GHA | O | High-side gate driver output. Connect to the gate of the high-side power MOSFET |
7 | SHA | I | High-side source sense input. Connect to the high-side power MOSFET source. If high-side power MOSFET is not used, connect to GND |
8 | DLA | I | Low-side MOSFET drain sense input. Connect to the low-side MOSFET drain |
9 | GLA | O | Low-side gate driver output. Connect to the gate of the low-side power MOSFET |
10 | SLA | I | Low-side source sense input. Connect to the low-side power MOSFET source |
11 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
12 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
13 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
14 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
15 | SLB | I | Low-side source sense input. Connect to the low-side power MOSFET source |
16 | GLB | O | Low-side gate driver output. Connect to the gate of the low-side power MOSFET |
17 | DLB | I | Low-side MOSFET drain sense input. Connect to the low-side MOSFET drain |
18 | SHB | I | High-side source sense input. Connect to the high-side power MOSFET source. If high-side power MOSFET is not used, connect to GND |
19 | GHB | O | High-side gate driver output. Connect to the gate of the high-side power MOSFET |
20 | GHC | O | High-side gate driver output. Connect to the gate of the high-side power MOSFET |
21 | SHC | I | High-side source sense input. Connect to the high-side power MOSFET source. If high-side power MOSFET is not used, connect to GND |
22 | DLC | I | Low-side MOSFET drain sense input. Connect to the low-side MOSFET drain |
23 | GLC | O | Low-side gate driver output. Connect to the gate of the low-side power MOSFET |
24 | SLC | I | Low-side source sense input. Connect to the low-side power MOSFET source |
25 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
26 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
27 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
28 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
29 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
30 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
31 | nFAULT | OD | Fault indicator output. This pin is pulled logic low during a fault condition and requires an external pullup resistor |
32 | SDO | PP | Serial data output. Data is shifted out on the rising edge of the SCLK pin. VSDO determines logic level on the output |
33 | SDI | I | Serial data input. Data is captured on the falling edge of the SCLK pin |
34 | SCLK | I | Serial clock input. Serial data is shifted out and captured on the corresponding rising and falling edge on this pin |
35 | nSCS | I | Serial chip select. A logic low on this pin enables serial interface communication |
36 | ENABLE | I | Gate driver enable. When this pin is logic low the device goes to a low-power sleep mode. An 20-μs (typ) low pulse can be used to reset fault conditions |
37 | NC | NC | No internal connection. This pin can be left floating or connected to system ground. |
38 | AGND | PWR | Device analog ground. Connect to system ground |
39 | DVDD | PWR | 3.3-V internal regulator output. Connect a bypass capacitor between the DVDD and AGND pins. This regulator can externally source up to 30 mA. |
40 | VSDO | PWR | Supply pin for SDO output. Connect to 5-V or 3.3-V depending on the desired logic level. Connect a bypass capacitors between VSDO and AGND |
41 | INHA | I | High-side gate driver control input. This pin controls the output of the high-side gate driver |
42 | INLA | I | Low-side gate driver control input. This pin controls the output of the low-side gate driver |
43 | INHB | I | High-side gate driver control input. This pin controls the output of the high-side gate driver |
44 | INLB | I | Low-side gate driver control input. This pin controls the output of the low-side gate driver |
45 | INHC | I | High-side gate driver control input. This pin controls the output of the high-side gate driver |
46 | INLC | I | Low-side gate driver control input. This pin controls the output of the low-side gate driver |
47 | PGND | PWR | Device power ground. Connect to system ground |
48 | NC | NC | No connect. Do not connect anything to this pin |
— | Thermal Pad | PWR | Must be connected to ground |