ZHCSIU4A September 2018 – August 2019 ADS1284
PRODUCTION DATA.
The ADS1284 can perform very power-efficient, one-shot conversions using the STANDBY command while under software control. Figure 63 shows this sequence. First, issue the STANDBY command to set the standby mode.
When ready to make a measurement, issue the WAKEUP command. When DRDY goes low, the fully-settled conversion data are ready and can be read directly in read-data-continuous mode. Afterwards, issue another STANDBY command. When ready for the next measurement, repeat the cycle starting with another WAKEUP command.