ZHCZ035D November 2023 – May 2026 AM263P2-Q1 , AM263P4 , AM263P4-Q1
CONTROLSS-ADC:如果未设置 INTxCONT(继续中断模式),中断可能会停止
在 ADCINTSELxNx[INTxCONT]= 0 时,设置 ADCINTFLG 后,中断将停止,并且不会发生其他 ADC 中断。若在 ADCINTFLGCLR 寄存器进行软件写入的同时发生 ADC 中断,则 ADCINTFLG 将意外保持为设置状态,阻止将来发生 ADC 中断。
ADCINTSEL1N2[INT1CONT] = 1;
ADCINTSEL1N2[INT2CONT] = 1;
ADCINTSEL3N4[INT3CONT] = 1;
ADCINTSEL3N4[INT4CONT] = 1;AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
if(1 == AdcaRegs.ADCINTOVF.bit.ADCINT1) //ADCINT overflow
{
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 again
// If the ADCINTOVF condition will be ignored by the application
// then clear the flag here by writing 1 to ADCINTOVFCLR.
// If there is a ADCINTOVF handling routine, then either insert
// that code and clear the ADCINTOVF flag here or do not clear
// the ADCINTOVF here so the external routine will detect the
// condition.
// AdcaRegs.ADCINTOVFCLR.bit.ADCINT1 = 1; // clear OVF