ZHCSSH5A August 2023 – December 2024 LOG200
PRODMIX
The following figures show oscilloscope captures of the LOG200 output as the device responds to one-decade shifts in the input current. Rising and falling steps between 10nA and 100nA, and between 10µA and 100µA, were recorded. The oscilloscope was set to use the ac-coupled path.
For the current steps between 10nA and 100nA, a 10mA laser diode bias was used. A rise time of approximately 268ns and a fall time of approximately 626ns are observed.
Figure 7-6 10nA-to-100nA Current
Step
Figure 7-7 100nA-to-10nA Current StepFor the current steps between 10µA and 100µA, a 13mA laser diode bias was used. A rise time of approximately 45.60ns and a fall time of approximately 55.60ns are observed.
Figure 7-8 10µA-to-100µA Current
Step
Figure 7-9 100µA-to-10µA Current
Step