ZHCAAU5 October 2020 TMP61 , TMP61-Q1 , TMP63 , TMP63-Q1 , TMP64 , TMP64-Q1
// (2) Method two will read the ADC and insert that value into the FIFO N times as set in "#define Tmp_1_length" then average the values
// FIFO setup of the temporary arrays and define the filter depth (samples to average)
#define Tmp_1_length 16 // Sample length for the averaging filter for oversampling
Float Tmp_1_array[Tmp_1_length]; // The FIFO arrays for averaging the ADC value
float ADC_AVG = 0; // This is the averaged ADC value over (x) samples
float ADC_Value = 0; // This is the most recent ADC value captured
int i = 0; // set to 0 for the array position counter
float sum_array_1 = 0; // set to 0
int j = 0; // set to 0 for the sample counter
void FIFO_AVG(void)
{
// FIFO to average thermistor temperature
i = 0; // reset to 0
j = 0; // reset to 0
sum_array_1 = 0; // reset to 0
for (j = 0; j < Tmp_1_Length - 1; i++) // shift the array as a FIFO and drop the last data value, add the new value to the array for (x) samples
{
// read the ADC and put the new value into the ADC_Value register
for (i = 0; i < Tmp_1_length - 1; i++) // shift the array as a FIFO and drop the last data value
{
Tmp_1_array[i] = Tmp_1_array[i + 1]; // makes all the array indexes equal to the number after them
}
Tmp_1_array[Tmp_1_length - 1] = ADC_Value; // add the new value to the beginning of the array
for (i = 0; i < Tmp_1_length; i++) // sum the array
{
sum_array_1 += Tmp_1_array[i]; // add all of the array elements
}
ADC_AVG = sum_array_1 / Tmp_1_length; // divide the sum of the array to get an average
// Call the FIFO_AVG routine to get N ADC values averaged
FIFO_AVG();
// The ADC average value will be placed into ADC_AVG register