TIDT434 February 2025
The maximum voltage stress on the drain of the low-side FETs (Q2 and Q3) occurs with 150V input and 10A load. This was recorded as 170Vpk, as shown in Figure 3-1 and Figure 3-2.
Figure 3-1 Maximum Voltage Stress, 150VIN, 10A Load
Figure 3-2 Switch Node, 150VIN, 10A Load