TIDT417 November 2024
Output voltage ripple is shown in Figure 3-2 and Figure 3-3, where VSYS equals 3.75V and ISYS equals 3A. Note that the oscillations in the output voltage ripple are inherent to the BQ25638 and the small inductor value. The device outputs a 3.75VDC within reason.
Figure 3-2 Output Voltage Ripple at VBUS = 5V
Figure 3-3 Output Voltage Ripple at VBUS = 9V