TIDT375 December 2023
The board in the test jig with the heat sink mounted is shown in the following figure.
Figure 1-3 Test SetupThe fan
used in the tests was PFB0412EN-E from Delta. This fan runs on 12 V with an input current
draw of
2.6 A and a maximum air flow of 38 CFM.
Figure 1-4 Test Connections