SWRU556 June   2021 CC3100 , CC3200

 

  1.   Trademarks
  2. 1 Introduction
  3. 2 Features
  4. 3 Prerequisites
    1. 3.1 Software Downloads
    2. 3.2 Hardware
  5. 4 Radio Tool Installation Directory
  6. 5 Hardware Connections
    1. 5.1 CC31xxBOOST Plus CC31XXEMUBOOST
      1. 5.1.1 Using the UART Interface
      2. 5.1.2 Using the SPI Interface
    2. 5.2 CC32xx-LAUNCHXL
  7. 6 Flashing the Board
  8. 7 Running the RadioTool GUI
    1. 7.1 Set Up Tab and General Information
    2. 7.2 GUI TX Testing
    3. 7.3 GUI RX Testing
  9. 8 Current Measurement
  10. 9 CLI Version
  11. 10Insertion Loss Calibration
  12. 11Hardware Connections on Non-TI EVMs
  13. 12Source Code for Developers
    1. 12.1 RadioTool Application Sources
    2. 12.2 CC32xx Application Source

CC32xx-LAUNCHXL

Connect the RF connector to a WLAN tester/RF equipment for measurements, and the USB connector on the CC32xx LaunchPad™ to the PC. Ensure the RF connection to the instrument is made before powering on the board, so that the correct load impedance is provided during power on.

By default, the RF path is routed to J11 (Murata RF Switch). If users want to use J10 (uFL) for RF measurements, swap the position of the 0-Ω resistor to disconnect the path to the onboard antenna, and enable the path to the uFL connector.

The LaunchPad enumerates COM ports in the Device Manager on the PC, as shown in Figure 5-4. Keep a record of the Application/User UART port number, because it is needed later for the connection.

While using TI's XDS LaunchPad, the RadioTool GUI should automatically detect the correct UART number and set it on the GUI on the "COM Port" combo box.

GUID-27D248E5-74FA-4BA8-965D-25F76B05A266-low.gif Figure 5-4 XDS Connection Ports for CC32xx LaunchPad