SWRU467A February   2017  – June 2018 CC3120

 

  1.   CC3120 SimpleLink™ Wi-Fi® Internet-on-a chip™ Solution SDK Getting Started Guide
    1.     Trademarks
    2. 1 Introduction
    3. 2 Prerequisites
      1. 2.1 Hardware
      2. 2.2 Software Installation
    4. 3 Board Configuration
      1. 3.1 Board Setup For Programming
      2. 3.2 Board Setup With An External MCU
    5. 4 Programming the CC3120 BoosterPack™
    6. 5 Getting Started With the MSP-EXP432P401R LaunchPad™
      1. 5.1 Connecting the CC3120BOOST or BOOSTXL-CC3120MOD Board With the MSP-EXP432P401R Board
      2. 5.2 Terminal Setting
      3. 5.3 SDK Installation
      4. 5.4 Setting Up Code Composer Studio™
        1. 5.4.1 CCS™ Installation
        2. 5.4.2 Post Code Composer Studio™ Installation Setup
        3. 5.4.3 Importing network_terminal Example in Code Composer Studio™
        4. 5.4.4 Compiling and Debugging the Project in Code Composer Studio™
      5. 5.5 Setting Up IAR Embedded Workbench® for ARM
        1. 5.5.1 IAR Installation
        2. 5.5.2 Post IAR Installation Setup
        3. 5.5.3 Importing the network_terminal Example in IAR
        4. 5.5.4 Compiling and Debugging the Project in IAR
    7. 6 Getting Started With SimpleLink™ Studio
      1. 6.1 Visual Studio Installation
      2. 6.2 Importing network_terminal Example in Visual Studio
      3. 6.3 Compiling and Debugging the Project in Visual Studio
  2.   Revision History

Software Installation

The user is expected to have the following:

This tutorial assumes the packages are installed at the default location. The paths for these installations may be different, depending on the version of the software you downloaded. Regardless, users can manually define these paths without affecting the overall experience.

If FTDI drivers are not installed on your Windows PC, install the drivers when prompted by the SDK installer.