SWRU467A February   2017  – June 2018 CC3120

 

  1.   CC3120 SimpleLink™ Wi-Fi® Internet-on-a chip™ Solution SDK Getting Started Guide
    1.     Trademarks
    2. 1 Introduction
    3. 2 Prerequisites
      1. 2.1 Hardware
      2. 2.2 Software Installation
    4. 3 Board Configuration
      1. 3.1 Board Setup For Programming
      2. 3.2 Board Setup With An External MCU
    5. 4 Programming the CC3120 BoosterPack™
    6. 5 Getting Started With the MSP-EXP432P401R LaunchPad™
      1. 5.1 Connecting the CC3120BOOST or BOOSTXL-CC3120MOD Board With the MSP-EXP432P401R Board
      2. 5.2 Terminal Setting
      3. 5.3 SDK Installation
      4. 5.4 Setting Up Code Composer Studio™
        1. 5.4.1 CCS™ Installation
        2. 5.4.2 Post Code Composer Studio™ Installation Setup
        3. 5.4.3 Importing network_terminal Example in Code Composer Studio™
        4. 5.4.4 Compiling and Debugging the Project in Code Composer Studio™
      5. 5.5 Setting Up IAR Embedded Workbench® for ARM
        1. 5.5.1 IAR Installation
        2. 5.5.2 Post IAR Installation Setup
        3. 5.5.3 Importing the network_terminal Example in IAR
        4. 5.5.4 Compiling and Debugging the Project in IAR
    7. 6 Getting Started With SimpleLink™ Studio
      1. 6.1 Visual Studio Installation
      2. 6.2 Importing network_terminal Example in Visual Studio
      3. 6.3 Compiling and Debugging the Project in Visual Studio
  2.   Revision History

Compiling and Debugging the Project in IAR

For the debug session, complete the following steps:

  1. Select Project → options from the menu, and select the Debugger category. In the Setup tab, choose TI XDS as the driver and click OK (see Figure 30).
  2. IAR_TI_XDS_debugger.gifFigure 30. IAR TI XDS Debugger
  3. Go to the TI XDS category, choose TI XDS110 Emulator as the emulator and JTAG (4-pin) as the interface (see Figure 31).
  4. IAR_XDS110_debugger.gifFigure 31. IAR XDS110 Debugger
  5. Check the Use flash loader(s) checkbox in the Debugger → Download tab (see Figure 32).
  6. IAR_debugger_settings.gifFigure 32. IAR Debugger Settings
  7. Start debugging by clicking the green arrow on the top of the window to start the debugger.