SWRU467A February   2017  – June 2018 CC3120

 

  1.   CC3120 SimpleLink™ Wi-Fi® Internet-on-a chip™ Solution SDK Getting Started Guide
    1.     Trademarks
    2. 1 Introduction
    3. 2 Prerequisites
      1. 2.1 Hardware
      2. 2.2 Software Installation
    4. 3 Board Configuration
      1. 3.1 Board Setup For Programming
      2. 3.2 Board Setup With An External MCU
    5. 4 Programming the CC3120 BoosterPack™
    6. 5 Getting Started With the MSP-EXP432P401R LaunchPad™
      1. 5.1 Connecting the CC3120BOOST or BOOSTXL-CC3120MOD Board With the MSP-EXP432P401R Board
      2. 5.2 Terminal Setting
      3. 5.3 SDK Installation
      4. 5.4 Setting Up Code Composer Studio™
        1. 5.4.1 CCS™ Installation
        2. 5.4.2 Post Code Composer Studio™ Installation Setup
        3. 5.4.3 Importing network_terminal Example in Code Composer Studio™
        4. 5.4.4 Compiling and Debugging the Project in Code Composer Studio™
      5. 5.5 Setting Up IAR Embedded Workbench® for ARM
        1. 5.5.1 IAR Installation
        2. 5.5.2 Post IAR Installation Setup
        3. 5.5.3 Importing the network_terminal Example in IAR
        4. 5.5.4 Compiling and Debugging the Project in IAR
    7. 6 Getting Started With SimpleLink™ Studio
      1. 6.1 Visual Studio Installation
      2. 6.2 Importing network_terminal Example in Visual Studio
      3. 6.3 Compiling and Debugging the Project in Visual Studio
  2.   Revision History

Board Setup With An External MCU

The CC3120 BoosterPack evaluation board requires a host MCU to execute the user application. This guide uses the MSP-EXP432P401R LaunchPad as a reference.

Figure 8 shows how the MSP-EXP432P401R LaunchPad jumpers must be configured.

MSP-EXP432P401R_with_jumper_configuration.gifFigure 8. MSP-EXP432P401R With Jumper Configuration

Figure 9 shows how to mount the CC3120BOOST board on top of the MSP-EXP432P401R board. Ensure P1.1 of both boards are aligned with each other, as indicated by the white arrows on both boards. The micro USB connector on the MSP-EXP432P401R board is used as the power source and also as the programming interface for the user application.

CC31XXBOOST_mounted_on_MSP-EXP432P401R.gifFigure 9. CC3120BOOST Board Mounted on Top of the MSP-EXP432P401R Board