SPRZ487D May   2022  – December 2023 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2351
      2.      i2372
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2097
      4.      i2103
      5.      i2134
      6.      i2189
      7.      i2196
      8.      i2232
      9.      i2244
      10.      i2310
      11.      i2311
      12.      i2327
      13.      i2328
      14.      i2279
      15.      i2307
      16.      i2320
      17.      i2329
      18.      i2208
      19.      i2249
      20.      i2278
      21.      i2312
      22.      i2366
      23.      i2371
      24.      i2253
      25.      i2283
      26.      i2383
      27.      i2401
      28.      i2407
      29.      i2409
      30.      i2410
  4.   Trademarks
  5.   Revision History

i2407

RESET: MCU_RESETSTATz unreliable when MCU_RESETz is asserted low

Details:

MCU_RESETSTATz goes high periodically for a short duration and then low again while MCU_RESETz is still asserted low. This issue is seen only when MCU_RESETz is asserted low for greater than 100us. The device remains in reset while MCU_RESETz is low; the advisory only applies to the signal MCU_RESETSTATz.

Workaround(s):

Any one of the following could be used as a workaround for this advisory

  • Do not use MCU_RESETz in a functional system. MCU_RESETz can still be used for debug, realizing the errata limitation.
  • Limit the maximum low duration of MCU_RESETz to less than 100us.
  • Use Main Domain RESETSTATz instead of MCU_RESETSTATz. MCU_RESETz also causes a Main reset, so Main Domain RESETSTATz could be used for device reset observation. Consult the datasheet for RESETSTATz timing specifications.
  • For new designs, the circuits which produce Main Domain reset and MCU Domain reset should be combined with an AND gate as an input to RESETz. Also connect MCU Domain reset circuit to the MCU_RESETz input. This will provide full functionality of MCU warm reset using MCU_RESETz and MCU_RESETSTATz to indicate status of MCU domain reset. RESETz will be triggered on either a MAIN domain reset or MCU domain reset by using the AND gate.