SPRZ357P August 2011 – June 2020 F28M35E20B , F28M35H22C , F28M35H52C , F28M35H52C-Q1 , F28M35M22C , F28M35M52C
Table 5 shows which silicon revision(s) are affected by each advisory.
| TITLE | SILICON REVISION(S) AFFECTED | |||
|---|---|---|---|---|
| 0 | A | B | E | |
| Analog Subsystem: Analog Subsystem Function InitAnalogSystemClock() is Incomplete | Yes | Yes | Yes | Yes |
| Analog Subsystem: Potential Race Condition after Executing Analog Subsystem Functions AnalogClockEnable() or AnalogClockDisable() | Yes | Yes | Yes | Yes |
| ADC: Initial Conversion | Yes | Yes | Yes | Yes |
| ADC: ADC Result Conversion When Sampling Ends on 14th Cycle of Previous Conversion, ACQPS = 6 or 7 | Yes | Yes | Yes | Yes |
| ADC: Offset Self-Recalibration Requirement | Yes | Yes | Yes | Yes |
| ADC: ADC can Become Non-Responsive When ADCNONOVERLAP or RESET is Written During a Conversion | Yes | Yes | Yes | Yes |
| VREG: VREG 'Warn Lo/High' Feature Does Not Work as Intended | Yes | Yes | Yes | Yes |
| VREG: VREG Will be Enabled During Power Up Irrespective of VREG12EN | Yes | Yes | Yes | Yes |
| UART: RTRIS Bit in the UARTRIS Register is Only Set When the Interrupt is Enabled | Yes | Yes | Yes | Yes |
| System Control: Clock Configuration Should Not be Changed When There are Pending or On-going Accesses to Shared RAM (Cx and Sx) or to Analog Subsystem | Yes | Yes | Yes | Yes |
| SSI: SSI Microwire Frame Format is Not Supported on This Device | Yes | Yes | Yes | Yes |
| ePWM: ePWM7 is Clocked by CPUCLK and Will Stop During IDLE | Yes | Yes | Yes | Yes |
| ePWM: ePWM Dead-Band Delay Value Cannot be Set to 0 When Using Shadow Load Mode for RED/FED | Yes | Yes | Yes | Yes |
| ePWM: An ePWM Glitch can Occur if a Trip Remains Active at the End of the Blanking Window | Yes | Yes | Yes | Yes |
| ePWM: Trip Events Will Not be Filtered by the Blanking Window for the First 3 Cycles After the Start of a Blanking Window | Yes | Yes | Yes | Yes |
| Missing Clock Detect: Slow Crystal Start-up Can Cause a Missing Clock Detect Without an Interrupt | Yes | Yes | Yes | Yes |
| Missing Clock Detect: Watchdog and NMI Watchdog Resets Will be Persistent While X1 Clock is Absent | Yes | Yes | Yes | Yes |
| FPU: CPU-to-FPU Register Move Operation Followed By F32TOUI32, FRACF32, or UI16TOF32 Operations | Yes | Yes | Yes | Yes |
| FPU: FPU-to-CPU Register Move Operation Preceded by Any FPU 2p Operation | Yes | Yes | Yes | Yes |
| Memory: Prefetching Beyond Valid Memory | Yes | Yes | Yes | Yes |
| Flash Pump Power Down: Software Sequence Must be Followed to Power Down the Flash Pump | Yes | |||
| HWBIST: Maximum Frequency | Yes | Yes | Yes | Yes |
| HWBIST: Unexpected Behavior When C28x HWBIST is Run With EPI Enabled | Yes | Yes | Yes | Yes |
| HWBIST: C28x HWBIST Restriction on Real-Time Window of EPI Module | Yes | Yes | Yes | |
| HWBIST: C28x HWBIST Restriction on EPI Module | Yes | Yes | Yes | |
| HWBIST: C28x HWBIST Should Not be Used | Yes | Yes | Yes | |
| RAM Controller: Cortex-M3 Correctable Error Address Register Always has Value 0x0 | Yes | Yes | Yes | Yes |
| RAM Controller: C28x Correctable Error Address Register Always has Value 0x0 | Yes | |||
| RAM Controller: Cortex-M3 Accesses to Shared RAM (Cx and Sx) and to MSG RAM Do Not Work When Any Other Master (μDMA/C28x/DMA) Simultaneously Accesses the Same Memory | Yes | |||
| RAM Controller: μDMA Accesses to Shared RAM (Cx and Sx) and to MSG RAM Do Not Work When Any Other Master (Cortex-M3/C28x/DMA) Simultaneously Accesses the Same Memory | Yes | |||
| eQEP: eQEP Inputs in GPIO Asynchronous Mode | Yes | Yes | Yes | Yes |
| eQEP: Position Counter Incorrectly Reset on Direction Change During Index | Yes | Yes | Yes | Yes |
| eQEP: Missed First Index Event | Yes | |||
| GPIO: GPIO38 and GPIO46 Signal Latch-up to VSS Due to Fast Transient Sensitivity at High Temperature | Yes | Yes | Yes | Yes |
| Master Subsystem GPIO: Open-Drain Configuration May Drive a Short High Pulse | Yes | Yes | Yes | Yes |
| GPIO: Pins GPIO38 and GPIO46 Cannot be Used for Functions Other Than USB | Yes | |||
| GPIO: GPIOs on Port C Do Not Toggle Correctly When Using the GPCTOGGLE Register | Yes | |||
| GPIO: Cortex-M3/C28x Reads GPIO State as ‘0’ When the GPIO is Mapped to the Other Core | Yes | |||
| Control Subsystem I2C: FIFO Interrupt Trigger Levels Capped at 7 | Yes | Yes | Yes | Yes |
| Control Subsystem: Reset Value (/8) of CCLKCTL.CLKDIV Bit Field Violates the MIN Requirement Mandated by the Data Manual for ACIBCLK, When the Input Clock to the Divider is Less Than 40 MHz | Yes | |||
| PLL: May Not Lock on the First Lock Attempt | Yes | Yes | Yes | Yes |
| PLL: Setting SYSPLLMULT or UPLLMULT to 0x0000 causes "/0" Condition in PLL Logic | Yes | |||
| PBIST: ROM Cannot be Accessed During PBIST Execution | Yes | Yes | Yes | Yes |
| PBIST: DCAN0 Memory Cannot be Tested in Stand-alone Configuration | Yes | |||
| C28x Flash: A Single-Bit ECC Error May Cause Endless Calls to Single-Bit-Error Interrupt Service Routine | Yes | Yes | Yes | Yes |
| C28x Flash: Code Executing From the C28x Subsystem Flash May be Subject to Unnecessary 1-Cycle Delays | Yes | |||
| C28x Flash: The SBF and BF Instructions Will Not Execute From Flash | Yes | |||
| Reset: XRS May Toggle During Power Up | Yes | Yes | Yes | |
| Cortex-M3 Flash: C28x Reset While C28x Holding Pump Ownership Can Cause Erroneous Cortex-M3 Flash Reads | Yes | Yes | Yes | |
| Crystal: Maximum Equivalent Series Resistance (ESR) Values are Reduced | Yes | Yes | Yes | |
| USB/GPIO38: GPIO38/VBUS Cannot be Used as an Output | Yes | |||
| USB: VBUS Pin May Clamp to 3.3-V Supply, Preventing Proper OTG Mode Operation | Yes | |||
| USB: Host Mode — Cannot Communicate With Low-Speed Device Through a Hub | Yes | |||
| Debug: Cross-Trigger Functionality is Limited When Using Breakpoints on the C28x Core | Yes | |||
| Debug: Global Run of Cortex-M3 and TMS320C28x is not Operational | Yes | |||
| Debug: Control Subsystem Boot ROM M0 RAM-INIT Does Not Wait for RAM-INIT to Complete | Yes | |||
| NMI: Writing a "0" to Any of the CNMIFRC or MNMIFRC Register Bits Clears the Corresponding Flag Bit in CNMIFLG or MNMIFLG | Yes | |||
| Master Subsystem I2C: SDA and SCL Open-Drain Output Buffer Issue | Yes | Yes | Yes | Yes |
| Master Subsystem I2C: Data Hold Time Violates Philips® I2C Specification | Yes | |||
| Master Subsystem: MNMIFLG.NMIINT Bit Will Not be Set in Some Cases When an NMI is Still Pending | Yes | |||
| Master Subsystem MPU: Memory Protection Unit is Disabled | Yes | |||
| Master Subsystem Boot ROM: NMI Handler Can Return Before Clearing All the Pending NMIs, if There is a Nested NMI | Yes | |||
| Master Boot ROM: NMI Handler Not Executed if NMI Occurs at Power Up or Immediately After a Reset | Yes | |||
| Master Boot ROM: Parallel Boot Mode Will Not Work as Intended | Yes | |||
| C28x Clocking: EALLOW Protection of C28x Clocking Registers Prevents Read of Registers | Yes | |||
| μDMA: No Transfer Completion Interrupt From SW Channels, Other Than Channel 30 | Yes | |||
| VCU: First CRC Calculation May Not be Correct | Yes | |||
| Flash ECC: When Program/Data Cache is Enabled, ECC Errors are Captured Only on a Single 64-Bit Slice and Not on the Full 128-Bit Flash Bank Data Width | Yes | |||
| Flash ECC: C28x 'Flash Uncorrectable' Error Generated When Executing F021 Flash API Functions With Flash ECC Enabled | Yes | |||
| Temperature Sensor: getTempSlope() and getTempOffset() Functions are not Available on TMX Silicon | Yes | |||
| EMAC: Resetting EMAC Controller Using SRCR2 Register Does Not Automatically Reset the Ethernet PHY Via MII_PHYRST Signal | Yes | |||
| Read of Clock Control Registers on C28x Memory Map is EALLOW-Protected | Yes | |||
| CPU Self Test (HWBIST) is not Supported on Revision 0 Devices | Yes | |||
| EPI: C28x Access to the EPI Bus on the Device | Yes | |||
0, A, B, E
The factory function InitAnalogSystemClock() is provided for the purpose of configuring the clock ratio used by the Analog Subsystem and returning its status. A successful, properly configured device will return the success code 0xA005.
For affected devices, InitAnalogSystemClock() is missing one step, which may misconfigure the Analog Subsystem clocking scheme and return a code not equal to 0xA005.
A misconfigured Analog Subsystem clocking scheme may lead to random ACIB faults. Under such error conditions, all of the following symptoms are exhibited:
Manually complete the clock initialization sequence with an additional step in the user software immediately prior to calling the InitAnalogSystemClock() function from the Control Subsystem. This extra step is required for every instance where InitAnalogSystemClock() is called by user software.
The additional step will assign the value of 7 to the C28x memory space at address 0x4E58. The following code is an example of how the workaround can be implemented for a device where the desired clock ratio between the Control Subsystem and Analog Subsystem is 4-to-1:
*(unsigned int*)0x4E58 = 7;
(**InitAnalogSystemClock)(ACLKDIV4);
Once the workaround is in place, InitAnalogSystemClock() should be expected to return the success code of 0xA005 and no further actions will be necessary for proper ACIB behavior.
0, A, B, E
The factory functions AnalogClockEnable() and AnalogClockDisable() are provided for the purpose of configuring the peripheral clocks of the analog modules. When an analog clock configuration attempt succeeds, the function returns the value of 0.
Due to configuration latencies between the Control Subsystem and Analog Subsystem, the desired clock configuration will not be effective immediately after the function returns. A race condition may be encountered if user software attempts to use a module before the clock configuration is complete.
Further, the factory function InitAnalogSystemClock() expects that the analog clock configurations are static during execution. If AnalogClockEnable() or AnalogClockDisable() is executed immediately before InitAnalogSystemClock(), the initialization sequence may be corrupted because the analog clock configuration is not static during execution. For such a scenario, the return value of InitAnalogSystemClock() will not be 0xA005 as expected. If the initialization sequence is corrupted, the device may require a reset to recover from the error condition.
The AnalogClockEnable() and AnalogClockDisable() functions support back-to-back executions so a race condition between calls is not possible when these analog clock configuration functions are executed immediately after each other.
After executing one or more calls to AnalogClockEnable() or AnalogClockDisable(), flush the analog clock configuration sequence by executing the factory function ReadAnalogClockStatus().
The read operation of ReadAnalogClockStatus() is automatically queued behind pending analog clock configuration updates so its return from execution can be used to definitively verify that the desired clock configuration sequence has completed.
For example, the following code will enable the ADC module clocks with AnalogClockEnable() calls, and it will flush the clock configuration operations with ReadAnalogClockStatus() before resetting the ADC modules:
while((**AnalogClockEnable)(AnalogConfig1,ADC1_ENABLE));
while((**AnalogClockEnable)(AnalogConfig2,ADC2_ENABLE));
(**ReadAnalogClockStatus)(AnalogConfig2);
Adc1Regs.ADCCTL1.bit.RESET = 1;
Adc2Regs.ADCCTL1.bit.RESET = 1;
0, A, B, E
When the ADC conversions are initiated by any source of trigger in either sequential or simultaneous sampling mode, the first sample may not be the correct conversion result.
For sequential mode, discard the first sample at the beginning of every series of conversions. For instance, if the application calls for a given series of conversions, SOC0→SOC1→SOC2, to initiate periodically, then set up the series instead as SOC0→SOC1→SOC2→SOC3 and only use the last three conversions, ADCRESULT1, ADCRESULT2, ADCRESULT3, thereby discarding ADCRESULT0.
For simultaneous sample mode, discard the first sample of both the A and B channels at the beginning of every series of conversions.
User application should validate if this workaround is acceptable in their application.
This issue is fixed completely by writing a 1 to the ADCNONOVERLAP bit in the ADCTRL2 register, which only allows the sampling of ADC channels when the ADC is finished with any pending conversion.
0, A, B, E
Each on-chip ADC takes 13 ADC clock cycles to complete a conversion after the sampling phase has ended. The result is then presented to the bus controller on the 14th cycle post-sampling and latched on the 15th cycle into the ADC result registers. If the next conversion's sampling phase terminates on this 14th cycle, the results latched by the bus controller into the result register are not assured to be valid across all operating conditions.
Some workarounds are as follows:
0, A, B, E
The factory offset calibration from Device_cal() may not ensure that each ADC's offset remains within specifications under all operating conditions in the customer's system.
For more details on AdcxOffsetSelfCal(), refer to the “ADC Zero Offset Calibration” section in the Analog Subsystem chapter of the Concerto F28M35x Technical Reference Manual.
0, A, B, E
The ADC can get into a non-responsive state when the ADCCTL2[ADCNONOVERLAP] is modified while a conversion is in progress. When in this condition, no further conversion from the ADC will be possible without a device reset.
There are two different ways to cause this condition:
Follow this sequence to modify ADCCTL2[ADCNONOVERLAP] or write ADCCTL1[RESET]:
An example code follows.
EALLOW;
// Set all SOC trigger sources to software
AdcRegs.ADCSOC0CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC1CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC2CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC3CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC4CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC5CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC6CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC7CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC8CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC9CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC10CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC11CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC12CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC13CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC14CTL.bit. TRIGSEL = 0;
AdcRegs.ADCSOC15CTL.bit. TRIGSEL = 0;
// Set all ADCINTSOCSEL1/2 to 0.
AdcRegs.ADCINTSOCSEL1.bit.SOC0 = 0;
AdcRegs.ADCINTSOCSEL1.bit.SOC1 = 0;
AdcRegs.ADCINTSOCSEL1.bit.SOC2 = 0;
AdcRegs.ADCINTSOCSEL1.bit.SOC3 = 0;
AdcRegs.ADCINTSOCSEL1.bit.SOC4 = 0;
AdcRegs.ADCINTSOCSEL1.bit.SOC5 = 0;
AdcRegs.ADCINTSOCSEL1.bit.SOC6 = 0;
AdcRegs.ADCINTSOCSEL1.bit.SOC7 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC8 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC9 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC10 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC11 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC12 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC13 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC14 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC15 = 0;
// Ensure there is not another SOC pending
while (AdcRegs.ADCSOCFLG1.all != 0x0);
// Wait for conversions to complete
// Delay time based on ACQPS = 6 , ADCCTL2[CLKDIV2EN] = 1, ADCCTL2[CLKDIV4EN] = 0
// 7 + 13 ADC Clocks = 20 ADCCLKS -> 40 SYSCLKS
asm(" RPT#40||NOP");
// ADCCTL2[ADCNONOVERLAP] = <new value>;
// ADCCTL1[RESET] = 1;
EDIS;
0, A, B, E
The VREG "Warn Lo/High" feature should not be used or enabled in the device. Do not set the VREGWARNE bit in the MNMICFG register as it could negatively affect the VREG output voltage.
None
0, A, B, E
This advisory only applies to systems that tie the VREG12EN pin high and use an external regulator for the 1.2-V VDD supply.
During power up of the 3.3-V VDDIO, the internal Voltage Regulator (VREG) will be active until the 1.2-V VDD supply reaches approximately 0.7 V. After this time, the state of the VREG12EN pin will either keep the internal VREG active (if low) or disable the internal VREG (if high).
None
0, A, B, E
The RTRIS (UART Receive Time-Out Raw Interrupt Status) bit in the UART Raw Interrupt Status (UARTRIS) register should be set when a receive time-out occurs, regardless of the state of the RTIM enable bit in the UART Interrupt Mask (UARTIM) register. However, currently the RTIM bit must be set in order for the RTRIS bit to be set when a receive time-out occurs.
For applications that require polled operation, the RTIM bit can be set while the UART interrupt is disabled in the NVIC using the IntDisable(n) function in the StellarisWare® Peripheral Driver Library, where n is 21, 22, or 49, depending on whether UART0, UART1, or UART2 is used. With this configuration, software can poll the RTRIS bit, but the interrupt is not reported to the NVIC.
0, A, B, E
If the clock configuration is being changed (for example, changing the clock divider for Cortex-M3) when there is a pending or on-going access to Shared RAM (Cx/Sx) or to the Analog Subsystem, the access could generate an error.
Software should ensure that there is no pending or on-going access to Shared RAM or to the Analog Subsystem when the clock configuration is being changed.
0, A, B, E
The Synchronous Serial Interface (SSI) module does not support the Microwire frame format. SSI and SPI frame formats are not affected.
None
0, A, B, E
The ePWM7 is clocked by C28x CPUCLK. When the CPUCLK stops, ePWM7 will also stop. The C28x (and ePWM7) will stop during:
Other ePWM modules are clocked by SYSCLK, which does not stop during IDLE or debugger halt.
None. Use other ePWM modules if the IDLE mode is used or ePWM must remain active during debugger HALT.
0, A, B, E
ePWM dead-band delay value cannot be set to 0 when using Shadow Load Mode for rising-edge delay (RED) and falling-edge delay (FED).
This is for both RED and FED.
0, A, B, E
The blanking window is typically used to mask any PWM trip events during transitions which would be false trips to the system. If an ePWM trip event remains active for less than three ePWM clocks after the end of the blanking window cycles, there can be an undesired glitch at the ePWM output.
Figure 3 illustrates the time period which could result in an undesired ePWM output.
Figure 3. Undesired Trip Event and Blanking Window Expiration Figure 4 illustrates the two potential ePWM outputs possible if the trip event ends within 1 cycle before or 3 cycles after the blanking window closes.
Figure 4. Resulting Undesired ePWM Outputs Possible Extend or reduce the blanking window to avoid any undesired trip action.
0, A, B, E
The Blanking Window will not blank trip events for the first 3 cycles after the start of a Blanking Window. DCEVTFILT may continue to reflect changes in the DCxEVTy signals. If DCEVTFILT is enabled, this may impact subsequent subsystems that are configured (for example, the Trip Zone submodule, TZ interrupts, ADC SOC, or the PWM output).
Start the Blanking Window 3 cycles before blanking is required. If a Blanking Window is needed at a period boundary, start the Blanking Window 3 cycles before the beginning of the next period. This works because Blanking Windows persist across period boundaries.
0, A, B, E
If the X1 crystal oscillator is slow to start, a Missing Clock Detect (MCD) event can occur. This will switch the clock source to the internal 10-MHz INTOSC.
The Boot ROM NMI ISR to service the CLOCKFAIL clears the MNMIFLG[CLOCKFAIL] bit to prevent an NMIWD reset. On start-up, the application code will not have an opportunity to execute a custom NMIWD ISR since the interrupt has already been serviced. The MCLKSTS[MCLKFLG] will be set correctly and must be polled by software to detect the MCD condition on start-up.
Check the MCLKSTS[MCLKFLG] bit in the initialization code. The application should respond according to the system requirements of a missing clock source situation.
Most applications can tolerate a slow crystal start-up. For these applications, a Watchdog reset can be forced. A Watchdog reset will be held for 512 clocks on the X1 clock input and the device will be held in reset until the crystal is active.
0, A, B, E
The Watchdog and NMI Watchdog resets will always be asserted for 512 cycles of the external X1 clock source. If the X1 clock source is permanently absent, this will result in a persistent assertion of XRS low for a Missing Clock Detect (MCD) event.
NOTE: The term "Watchdog" in this advisory applies to all Cortex-M3 watchdog timers: MNMIWD, WDT0, and WDT1.
The application code should contain an NMIWD ISR, which properly shuts down the system when an MCD event occurs. NOTE: MCD switches the clock source to the
10-MHz INTOSC and code will be executed using this clock.
The NMIWD CLOCKFAIL ISR should:
NOTE: If the application response to an MCD must avoid putting the device in reset, then there is a window of vulnerability between the MCD and a Watchdog expiration. If a watchdog timer configured to cause a reset expires before the NMIWD ISR services the watchdog, a persistent reset cannot be avoided.
0, A, B, E
This advisory applies when the write phase of a CPU-to-FPU register write coincides with the execution phase of the F32TOUI32, FRACF32, or UI16TOF32 instructions. If the F32TOUI32 instruction execution and CPU-to-FPU register write operation occur in the same cycle, the target register (of the CPU-to-FPU register write operation) gets overwritten with the output of the F32TOUI32 instruction instead of the data present on the C28x data write bus. This scenario also applies to the following instructions:
A CPU-to-FPU register write must be followed by a gap of five NOPs or non-conflicting instructions before F32TOUI32, FRACF32, or UI16TOF32 can be used.
The C28x code generation tools v6.0.5 (for the 6.0.x branch), v6.1.2 (for the 6.1.x branch), and later check for this scenario.
Example of Problem:
SUBF32 R5H, R3H, R1H
|| MOV32 *--XAR4, R4H
EISQRTF32 R4H, R2H
UI16TOF32 R2H, R3H
MOV32 R0H, @XAR0 ; Write to R0H register
NOP ;
NOP ;
F32TOUI32 R1H, R1H ; R1H gets written to R0H
I16TOF32 R6H, R3H
Example of Workaround:
SUBF32 R5H, R3H, R1H
|| MOV32 *--XAR4, R4H
EISQRTF32 R4H, R2H
UI16TOF32 R2H, R3H
MOV32 R0H, @XAR0 ; Write to R0H register
NOP
NOP
NOP
NOP
NOP
F32TOUI32 R1H, R1H
I16TOF32 R6H, R3H
0, A, B, E
This advisory applies when a multi-cycle (2p) FPU instruction is followed by a FPU-to-CPU register transfer. If the FPU-to-CPU read instruction source register is the same as the 2p instruction destination, then the read may be of the value of the FPU register before the 2p instruction completes. This occurs because the 2p instructions rely on data-forwarding of the result during the E3 phase of the pipeline. If a pipeline stall happens to occur in the E3 phase, the result does not get forwarded in time for the read instruction.
The 2p instructions impacted by this advisory are MPYF32, ADDF32, SUBF32, and MACF32. The destination of the FPU register read must be a CPU register (ACC, P, T, XAR0...XAR7). This advisory does not apply if the register read is a FPU-to-FPU register transfer.
In the example below, the 2p instruction, MPYF32, uses R6H as its destination. The FPU register read, MOV32, uses the same register, R6H, as its source, and a CPU register as the destination. If a stall occurs in the E3 pipeline phase, then MOV32 will read the value of R6H before the MPYF32 instruction completes.
Example of Problem:
MPYF32 R6H, R5H, R0H ; 2p FPU instruction that writes to R6H
|| MOV32 *XAR7++, R4H
F32TOUI16R R3H, R4H ; delay slot
ADDF32 R2H, R2H, R0H
|| MOV32 *--SP, R2H ; alignment cycle
MOV32 @XAR3, R6H ; FPU register read of R6H
Figure 5 shows the pipeline diagram of the issue when there are no stalls in the pipeline.
Figure 5. Pipeline Diagram of the Issue When There are no Stalls in the Pipeline Figure 6 shows the pipeline diagram of the issue if there is a stall in the E3 slot of the instruction I1.
Figure 6. Pipeline Diagram of the Issue if There is a Stall in the E3 Slot of the Instruction I1 Treat MPYF32, ADDF32, SUBF32, and MACF32 in this scenario as 3p-cycle instructions. Three NOPs or non-conflicting instructions must be placed in the delay slot of the instruction.
The C28x Code Generation Tools v.6.2.0 and later will both generate the correct instruction sequence and detect the error in assembly code. In previous versions, v6.0.5 (for the 6.0.x branch) and v.6.1.2 (for the 6.1.x branch), the compiler will generate the correct instruction sequence but the assembler will not detect the error in assembly code.
Example of Workaround:
MPYF32 R6H, R5H, R0H
|| MOV32 *XAR7++, R4H ; 3p FPU instruction that writes to R6H
F32TOUI16R R3H, R4H ; delay slot
ADDF32 R2H, R2H, R0H
|| MOV32 *--SP, R2H ; delay slot
NOP ; alignment cycle
MOV32 @XAR3, R6H ; FPU register read of R6H
Figure 7 shows the pipeline diagram with the workaround in place.
Figure 7. Pipeline Diagram With Workaround in Place 0, A, B, E
The C28x CPU prefetches instructions beyond those currently active in its pipeline. If the prefetch occurs past the end of valid memory, then the CPU may receive an invalid opcode.
The prefetch queue is 8 x16 words in depth. Therefore, code should not come within 8 words of the end of valid memory. This restriction applies to all memory regions and all memory types (flash, OTP, SARAM) on the device. Prefetching across the boundary between two valid memory blocks is all right.
Example 1: M1 ends at address 0x7FF and is not followed by another memory block. Code in M1 should be stored no farther than address 0x7F7. Addresses 0x7F8-0x7FF should not be used for code.
Example 2: M0 ends at address 0x3FF and valid memory (M1) follows it. Code in M0 can be stored up to and including address 0x3FF. Code can also cross into M1 up to and including address 0x7F7.
E
On silicon revision E, there is a logic change to prevent one CPU from powering down the Flash Pump while the other CPU is using it.
As a consequence of this change, both the Cortex-M3 and the C28x CPU must each power down the Flash Pump without any Flash accesses in between. The Flash Pump will not enter low-power mode if this sequence is not followed.
The F28M3xx_examples_Dual\Sleep_Low_Power_Mode_Wakeup example in controlSUITE™ can be used as a reference.
Along with the automatic power down, the Flash bank can be forced into its low-power mode. To force the Flash to power down completely, execute the following procedure from RAM (and not from Flash):
The Cortex-M3 should notify the C28x that it has completed the above sequence. It should wait until the C28x completes steps 4, 5, and 6.
The C28x should notify the Cortex-M3 that it has completed the power-down sequence so that both subsystems may continue. Also note that the PUMPRDY bit in the M3-FMC register space can be used by the application software to identify the current power mode status of the pump. The PUMPRDY bit (and also PMPPWR bit) in the C28x-FMC cannot be used for that purpose.
0, A, B, E
The Cortex-M3 HWBIST and C28x HWBIST can only be run when both M3SSCLK and C28SYSCLK are at or below the maximum frequency given in Table 6.
Set the device clock frequencies per Table 6 if using HWBIST. The maximum frequency depends on if the C28x-to-Cortex-M3 clock ratio is 2:1 or 1:1, and if the HWBIST is executed on only one CPU or both CPUs.
For part numbers with lower maximum frequencies than shown in Table 6, the lower frequency that is in the F28M35x Concerto™ Microcontrollers Data Manual still applies.
| CLOCK | 1:1 C28SYSCLK-to-M3SSCLK Ratio | 2:1 C28SYSCLK-to-M3SSCLK Ratio | ||||
|---|---|---|---|---|---|---|
| Only C28x HWBIST | Only Cortex-M3 HWBIST | C28x and Cortex-M3 HWBIST | Only C28x HWBIST | Only Cortex-M3 HWBIST | C28x and Cortex-M3 HWBIST | |
| C28SYSCLK | 100 | 85 | 85 | 130 | 130 | 130 |
| M3SSCLK | 100 | 85 | 85 | 65 | 65 | 65 |
0, A, B, E
Execution of C28x HWBIST with EPI enabled could result in unexpected device behavior. This advisory does not apply if the EPI is disabled.
Either of two workarounds listed below must be implemented before initiating a C28x HWBIST test interval.
If the EPI interrupt (INT12.6) has been enabled in PIE in the C28x application, it must be disabled before starting HWBIST. After HWBIST completion, the user should clear the MEMPROTERR flag in the CEPISTATUS register and the status bit for INT6 in the PIEIFR12 register, and then reenable the PIE interrupt for EPI.
The EPI can be restored to its original configuration after the C28x completes the HWBIST test interval.
A, B, E
The Real-Time Window (RTW) module may get reset when a C28x HWBIST is in progress.
The RTW feature of the EPI must be disabled before executing a HWBIST. After executing the HWBIST, the RTW needs to be reconfigured.
A, B, E
The C28x and C28x DMA AHB bridge may get reset during HWBIST execution.
All pending EPI accesses should be completed from the C28x and C28x DMA, and the CEPISTATUS register should be cleared before entering HWBIST. There is no restriction on the Cortex-M3 use of the EPI during C28x HWBIST execution.
0, A, B
Using the HWBIST feature on the C28x CPU can cause unpredictable behavior in the C28x subsystem.
None. The C28x HWBIST should not be used on the revisions affected.
0, A, B, E
The Correctable Error Address Register should capture the address for which the correctable error (1-bit ECC error) occurred, but the Correctable Error Address Register mapped to the Cortex-M3 core will always have value 0x0.
None. The original intent of this register is to aid in debugging. Note that correctable errors do get corrected, so this erratum does not affect device functionality.
0
The Correctable Error Address Register should capture the address for which the correctable error (1-bit ECC error) occurred, but the Correctable Error Address Register mapped to the C28x core will always have value 0x0.
None. The original intent of this register is to aid in debugging. Note that correctable errors do get corrected, so this erratum does not affect device functionality.
0
If Cortex-M3 accesses Shared RAM (Cx and Sx) or MSG RAM when any other master (µDMA/C28x/DMA) accesses the same memory, data and parity may get corrupted in the memory.
When Cortex-M3 accesses Shared RAM or MSG RAM, no other master (µDMA/C28x/DMA) should access the same memory at that time.
This is fixed in Revision A silicon.
0
If µDMA accesses Shared RAM (Cx and Sx) or MSG RAM when any other master (Cortex-M3/C28x/DMA) accesses the same memory, data and parity may get corrupted in the memory.
When µDMA accesses Shared RAM or MSG RAM, no other master (Cortex-M3/C28x/DMA) should access the same memory at that time.
This is fixed in Revision A silicon.
0, A, B, E
If any of the eQEP input pins are configured for GPIO asynchronous input mode via the GPxQSELn registers, the eQEP module may not operate properly. For example, QPOSCNT may not reset or latch properly, and pulses on the input pins may be missed. This is because the eQEP peripheral assumes the presence of external synchronization to SYSCLKOUT on inputs to the module.
For proper operation of the eQEP module, input GPIO pins should be configured via the GPxQSELn registers for synchronous input mode (with or without qualification). This is the default state of the GPxQSEL registers at reset. All existing eQEP peripheral examples supplied by TI also configure the GPIO inputs for synchronous input mode.
The asynchronous mode should not be used for eQEP module input pins.
Configure GPIO inputs configured as eQEP pins for non-asynchronous mode (any GPxQSELn register option except “11b = Asynchronous”).
0, A, B, E
While using the PCRM = 0 configuration, if the direction change occurs when the index input is active, the position counter (QPOSCNT) could be reset erroneously, resulting in an unexpected change in the counter value. This could result in a change of up to ±4 counts from the expected value of the position counter and lead to unexpected subsequent setting of the error flags.
While using the PCRM = 0 configuration [that is, Position Counter Reset on Index Event (QEPCTL[PCRM] = 00)], if the index event occurs during the forward movement, then the position counter is reset to 0 on the next eQEP clock. If the index event occurs during the reverse movement, then the position counter is reset to the value in the QPOSMAX register on the next eQEP clock. The eQEP peripheral records the occurrence of the first index marker (QEPSTS[FIMF]) and direction on the first index event marker (QEPSTS[FIDF]) in QEPSTS registers. It also remembers the quadrature edge on the first index marker so that same relative quadrature transition is used for index event reset operation.
If the direction change occurs while the index pulse is active, the module would still continue to look for the relative quadrature transition for performing the position counter reset. This results in an unexpected change in the position counter value.
The next index event without a simultaneous direction change will reset the counter properly and work as expected.
Do not use the PCRM = 0 configuration if the direction change could occur while the index is active and the resultant change of the position counter value could affect the application.
Other options for performing position counter reset, if appropriate for the application [such as Index Event Initialization (IEI)], do not have this issue.
0
If the first index event edge at the QEPI input occurs at any time from one system clock cycle before the corresponding QEPA/QEPB edge to two system clock cycles after the corresponding QEPA/QEP edge, then the eQEP module may miss this index event. This can result in the following behavior:
Reliable operation is achieved by delaying the index signal such that the QEPI event edge occurs at least two system clock cycles after the corresponding QEPA/QEPB signal edge. For cases where the encoder may impart a negative delay (td) to the QEPI signal with respect to the corresponding QEPA/QEPB signal (that is, QEPI edge occurs before the corresponding QEPA/QEPB edge), the QEPI signal should be delayed by an amount greater than "td + 2*SYSCLKOUT".
This is fixed in Revision A silicon.
0, A, B, E
There is a potential signal latch-up to VSS condition identified on pins GPIO38 and GPIO46. In this condition, an on-chip path to VSS is turned on, which can bring down the logic level of these pins below VIL and VOL. The condition can occur when the pin is in input or output mode and with any of the alternate functions muxed on to this pin.
The condition is more likely to occur at high temperatures and has not been observed below 85°C under normal operating use cases. The triggering event is dependent on board design and the speed of signals switching on these pins, with fast-switching transients more likely to induce the condition. The condition has only been observed when the signal at the device pin has a rise time or fall time faster than 2 ns (measured 10% to 90% of VDDIO).
The condition will resolve upon toggle of the IO at a lower temperature.
Try one of these two options:
Avoid the use of these pins in the revisions affected.
This condition is not seen on all products. Many PCB designs have enough capacitance and slow enough edge rates that the condition does not occur. If the application can be tested and functions correctly with the temperature margin above the end-use temperature, then no action may be required. If the issue is seen or additional margin is desired, then the following can be applied.
If the pin is configured as an output without any other pullup or driver connected:
If the pin is configured as an input:
0, A, B, E
Each GPIO can be configured to an open-drain mode using the GPIOODR register. (Note that the open-drain feature is only supported on Master Subsystem GPIOs.) However, an internal device timing issue may cause the GPIO to drive a logic-high for up to 0–10 ns during the transition into or out of the high-impedance state.
This undesired high-level may cause the GPIO to be in contention with another open-drain driver on the line if the other driver is simultaneously driving low. The contention is undesirable because it applies stress to both devices and results in a brief intermediate voltage level on the signal. This intermediate voltage level may be incorrectly interpreted as a high level if there is not sufficient logic-filtering present in the receiver logic to filter this brief pulse.
If contention is a concern, do not use the open-drain functionality of the GPIOs; instead, emulate open-drain mode in software. Open-drain emulation can be achieved by setting the GPIO data (GPIODATA) to a static 0 and toggling the GPIO direction bit (GPIODIR) to enable and disable the drive low.
0
Pins GPIO38 and GPIO46 can only be used as USB0VBUS and USB0ID. GPIO and other functions are not available.
None. This is fixed in Revision A silicon.
0
GPIOs on Port C do not toggle correctly when using the GPCTOGGLE register because of a dependency on the state of GPIOs on Port A.
Use GPCSET and GPCCLEAR registers or the GPCDAT register to toggle Port C GPIOs.
This is fixed in Revision A silicon.
0
The Cortex-M3 core reads the GPIO state as ‘0’ when the GPIO is mapped to the C28x core. Conversely, the C28x core reads the GPIO state as ‘0’ when the GPIO is mapped to the Cortex-M3 core.
None. This is fixed in Revision A silicon.
0, A, B, E
The TXFFIL (Transmit FIFO Interrupt Level) bits in the I2C Transmit FIFO (I2CFFTX) register and the RXFFIL (Receive FIFO Interrupt Level) bits in the I2C Receive FIFO (I2CFFRX) register are capped to a maximum value of 7. Writes of values greater than 7 to these fields will be truncated to the lower 3 bits.
Applications can poll the TXFFST (Transmit FIFO Status) and RXFFST (Receive FIFO Status) bits in the I2CFFTX and I2CFFRX registers, respectively, for an accurate count of the number of items in the FIFOs. Applications wishing to use I2C FIFO interrupts must set the interrupt levels to 7 or less.
0
On power up or after an external reset (XRS), PLL is bypassed and the Master Boot ROM configures the default SYSCLK divider to "/1". This makes the input clock to the divider the same as OSCCLK. If OSCCLK is less than 40 MHz, then upon power up or an external reset, ACIBCLK would be less than 5 MHz. However, this is not an issue because the Analog Subsystem needs not be functional during boot time.
An OTP function is provided in the Control Subsystem for users to call during their application initialization process and before using Analog Subsystem peripherals on the device. This function will configure the CCLKCTL divider as needed by the application.
This is fixed in Revision A silicon.
0, A, B, E
The PLL may not start properly at device power up. The PLLSTS[PLLLOCKS] lock counter bit is set, but the PLL does not produce a clock. Once the PLL has properly started, the PLL can be disabled and reenabled with no issues and will stay locked. However, the PLL lock problem could reoccur on a subsequent power-up cycle. If the PLLSYSCLK has not properly started and is selected as the CPU clock source, the CPU will stop executing instructions. The occurrence rate of this transient issue is low and after an initial occurrence, this issue may not be subsequently observed in the system again. Implementation of the workaround reduces the rate of occurrence.
This advisory applies to both PLLs.
System PLL Workaround
Repeated lock attempts will reduce the likelihood of seeing the condition on the final attempt. TI recommends a minimum of five lock sequences in succession when the PLL is configured the first time after a power up. A lock sequence means disabling the PLL, starting the PLL locking, and waiting for the PLLLOCKS lock counter bit to set. After the final sequence, the Watchdog is enabled and the clock source is switched to use the PLL output as normal.
The Watchdog timer is used to detect if the condition has occurred because it is not clocked by the PLL output. The Watchdog should be enabled before selecting the PLL as the clock source and configured to reset the device. If the PLL is not producing a clock, the Watchdog will reset the device and the user initialization software will therefore repeat the PLL initialization.
Many applications do not have a different initialization sequence for a Watchdog-initiated reset; for these applications, no further action is required. For applications that do use a different device initialization sequence when a Watchdog reset is detected, a flag can be set in RAM prior to initializing the PLL. This flag can be used to identify a PLL lock failure as the Watchdog reset cause and allow the retry to occur.
See the controlSUITE™ SysCtlClockPllConfig() function for an example implementation of this workaround.
The workaround can also be applied at the System level by a supervisor resetting the device if it is not responding.
USB PLL Workaround
The workaround for the USB PLL is similar to that for the System PLL except the Watchdog cannot be used to detect a PLL lock failure on the final attempt. The application must detect a USB clocking failure at the system level and issue a reset to the device for another USB PLL lock attempt.
See the controlSUITE SysCtlUSBPLLConfigSet() function for an example implementation of this workaround.
0
Setting the SYSPLLMULT register or UPLLMULT register to 0x0000 to bypass the PLL causes a "/0" condition in the PLL logic and results in an unstable PLL output clock.
Do not write 0x0000 to the SYSPLLMULT register or UPLLMULT register to bypass either PLLs. Instead, to bypass the system PLL, set SYSPLLCTL[SPLLCLKEN] = 0. To bypass the USB PLL, set UPLLCTL[UPLLCLKEN] = 0.
This is fixed in Revision A silicon.
0, A, B, E
During execution of a Cortex-M3 or C28x PBIST, all Cortex-M3 or C28x accesses to ROM on the device will fail. This does not impact a PBIST of the ROM itself, which will work as expected.
Do not access ROM during a PBIST execution.
0
If DCAN0 memory is run in stand-alone mode using the PBIST logic, it will generate a false fail regardless of memory integrity.
DCAN0 memory must be tested in distributed compare mode only. This is fixed in Revision A silicon.
0, A, B, E
When a single-bit ECC error is detected, the CPU executes the single-bit-error interrupt service routine (ISR). When the ISR returns, the same instruction that caused the first error is fetched again. If the ECC error threshold (ERR_THRESHOLD.THRESHOLD) is 0, then the same error is detected and another ISR is executed. This continues in an endless loop. This sequence of events only occurs if the error is caused by a program fetch operation, not a data read.
Set the error threshold bit-field (ERR_THRESHOLD.THRESHOLD) to a value greater than or equal to 1. Note that the default value of the threshold bit-field is 0.
0
Code executing from the C28x Subsystem Flash may be subject to unnecessary 1-cycle delays. This delay will not occur more often than once every 8 instructions for code that is composed of linear 32-bit opcodes with no pipeline delays (worst case). In practice, the unnecessary delay occurs rarely since the C28x uses both 16-bit opcodes and 32-bit opcodes.
This delay can occur when Flash wait states are set to "3" and the prefetch mechanism is enabled. This delay does not occur when the wait states are set to "2" or "1" with prefetch enabled.
None. This is fixed in Revision A silicon.
0
When the flash prefetch is enabled, the SBF and BF instructions will not be correctly fetched from the Flash.
Compile the application code with the –me option to avoid the SBF and BF instructions.
This is fixed in Revision A silicon.
0, A, B
During device power up, the XRS pin may toggle high prematurely. After the VDDIO and VDD supplies reach the recommended operating conditions, the XRS pin behavior will be as described in the F28M35x Concerto™ Microcontrollers Data Manual. This is only an issue with the external state of the XRS pin. Internally, the device will be held in reset until the supplies are within an acceptable range and XRS is high.
Disregard XRS activity on the board before the supplies reach the recommended operating conditions.
0, A, B
If the C28x Subsystem is reset while it owns the flash pump semaphore, then the flash pump itself will also reset. Since the flash pump is also used by the Cortex-M3 Subsystem, any instruction fetch or data read from flash by the Cortex-M3 will return invalid data. This will result in a hard fault, incorrect program execution, Cortex-M3 core hang condition, or an unspecified error in the application.
This erratum does not apply if the C28x Subsystem never writes to the CPUMPREQUEST register to take ownership of the flash pump semaphore.
The Cortex-M3 must not access flash while the C28x holds the flash pump semaphore ownership. The following steps describe how this can be achieved:
0, A, B
The maximum ESR values are reduced. For the revisions affected, the data in Table 7 supersedes the data given in the "Crystal Equivalent Series Resistance (ESR) Requirements" table in the F28M35x Concerto™ Microcontrollers Data Manual. The differences between the two tables are highlighted in Table 7.
| CRYSTAL FREQUENCY (MHz) | MAXIMUM ESR (Ω)
(CL1/2 = 12 pF) |
MAXIMUM ESR (Ω)
(CL1/2 = 24 pF) |
|---|---|---|
| 2 | 175 | 375 |
| 4 | 100 | 195 |
| 6 | 75 | 145 |
| 8 | 65 | 105 |
| 10 | 55 | 70 |
| 12 | 50 | 45 |
| 14 | 50 | 35 |
| 16 | 45 | 25 |
| 18 | 40 | 20 |
| 20 | 30 | 15 |
None
A
GPIO38 cannot be used as an output and may fail in the system if used as such at any time.
Do not use the output function on this pin. This is fixed in Revision B silicon.
0
The VBUS pin may clamp to VDDIO, preventing the pulldown resistors from taking effect in USB-OTG mode when attempting to end a session.
None. This is fixed in Revision A silicon.
0
When the USB controller is operating as a Host and a low-speed packet is sent to a device through a hub, the subsequent Start-of-Frame is corrupted. After a period of time, this corruption causes the USB controller to lose synchronization with the hub, which results in data corruption.
None. This is fixed in Revision A silicon.
0
When cross-triggering is enabled, halting at a breakpoint set for the C28x core does not also halt the Cortex-M3 core.
None. This is fixed in Revision A silicon.
0
Due to missing signals in the debug logic, global run of the Cortex-M3 and C28x cores is not enabled.
None. This is fixed in Revision A silicon.
0
C-Boot-ROM sets the RAM-INIT bit to zero-initialize the entire M0 RAM every time it is run after reset. However, it does not wait for the RAM-INIT to complete before accessing M0 RAM for run-time stack. This does not cause any problem on stand-alone device operation because this wait before RAM is accessed is inherently achieved by the wait to access Flash. As Flash power-up time is more than the M0 RAM-INIT time and the Boot ROM waits for Flash to power up completely before accessing RAM, by the time
C-Boot-ROM accesses M0 RAM for stack, it is initialized properly.
On stand-alone device operation, this is not a problem because every time the device is reset, Flash has to be brought back to active state and this wait for Flash to come to active state is more than the time required for M0 RAM-INIT to complete.
During debug or development, when the emulator is connected and the user wants to RUN through Boot ROM, care must be taken to ensure that Flash is not accessed before running through boot initialization or the user should carefully step through Boot ROM code at least until RAM-INIT is done, before clicking the RUN button on CCS.
This is fixed in Revision A silicon.
0
Writing a "0" to any of the bits in the Control Subsystem CNMIFRC register clears the corresponding bits in the CNMIFLG register. Likewise, writing a "0" to any of the bits in the Master Subsystem MNMIFRC register clears the corresponding bits in the MNMIFLG register.
Do not write "0" to any of the bits in the CNMIFRC register or MNMIFRC register. To clear the CNMIFLG and MNMIFLG bits, write a "1" to the corresponding bits in the respective CNMIFLGCLR and MNMIFLGCLR registers.
This is fixed in Revision A silicon.
0, A, B, E
The SDA and SCL outputs are implemented with push-pull 3-state output buffers rather than open-drain output buffers as required by I2C. While it is possible for the push-pull 3-state output buffers to behave as open-drain outputs, an internal timing skew issue causes the outputs to drive a logic-high for a duration of 0–5 ns before the outputs are disabled. The unexpected high-level pulse will only occur when the SCL or SDA outputs transition from a driven low state to a high-impedance state and there is sufficient internal timing skew on the respective I2C output.
This short high-level pulse injects energy in the I2C signals traces, which causes the I2C signals to sustain a period of ringing as a result of multiple transmission line reflections. This ringing should not cause an issue on the SDA signal because it only occurs at times when SDA is expected to be changing logic levels and the ringing will have time to damp before data is latched by the receiving device. The ringing may have enough amplitude to cross the SCL input buffer switching threshold several times during the first few nanoseconds of this ringing period, which may cause clock glitches. This ringing should not cause a problem if the amplitude is damped within the first 50 ns because I2C devices are required to filter their SCL inputs to remove clock glitches. Therefore, it is important to design the PCB signal traces to limit the duration of the ringing to less than 50 ns. One possible solution is to insert series termination resistors near the SCL and SDA terminals to attenuate transmission line reflections.
This issue may also cause the SDA output to be in contention with the slave SDA output for the duration of the unexpected high-level pulse when the slave begins its ACK cycle. This occurs because the slave may already be driving SDA low before the unexpected high-level pulse occurs. The glitch that occurs on SDA as a result of this short period of contention does not cause any I2C protocol issue but the peak current applies unwanted stress to both I2C devices and potentially increases power supply noise. Therefore, a series termination resistor located near the respective SDA terminal is required to limit the current during the short period of contention.
A similar contention problem can occur on SCL when connected to I2C slave devices that support clock stretching. This occurs because the slave is driving SCL low before the unexpected high-level pulse occurs. The glitch that occurs on SCL as a result of this short period of contention does not cause any I2C protocol issue because I2C devices are required to apply a glitch filter to their SCL inputs. However, the peak current applies unwanted stress to both I2C devices and potentially increases power supply noise. Therefore, a series termination resistor located near the respective SCL terminal is required to limit the current during the short period of contention.
If another master is connected, the unexpected high-level pulses on the SCL and SDA outputs can cause contention during clock synchronization and arbitration. The series termination resistors described above will also limit the contention current in this use case without creating any I2C protocol issue.
Insert series termination resistors on the SCL and SDA signals and locate them near the SCL and SDA terminals. The SCL and SDA pullup resistors should also be located near the SCL and SDA terminals. The placement of the series termination resistor and pullup resistor should be connected as shown in Figure 8.
Figure 8. Placement of Series Termination Resistor and Pullup Resistor Table 8 provides series termination and pullup resistor value recommendations. The I2C signal level and respective VDDIO power supply voltage is shown in the first column. Two resistor value combination options are provided for each voltage. One option supports a maximum high-level input current of 200 uA to all attached I2C devices, while the other option supports a maximum high-level input current of 100 uA to all attached I2C devices.
| I2C SIGNAL LEVEL AND RESPECTIVE VDDIO
POWER SUPPLY (V) |
SERIES TERMINATION RESISTOR (Ω) | PULLUP RESISTOR (Ω) | NOTES |
|---|---|---|---|
| 3.3 | 60 | 3300 | Maximum high-level input current up to 200 µA |
| 3.3 | 75 | 6600 | Maximum high-level input current up to 100 µA |
0
The Master subsystem I2C module’s data hold time on F28M35x Concerto devices is a minimum of 2 system clock cycles, which violates the Philips I2C specification requirement of a minimum of 0 system clock cycle.
None. This is fixed in Revision A silicon.
0
On the Master Subsystem, if there is a nested NMI and if the user clears the MNMIFLG.NMIINT bit before clearing all the other pending flags while returning from the first NMI handler, then the MNMIFLG.NMIINT bit will not be set while the second NMI is still pending. This pending NMI will keep the MNMIWD counter running and will reset the device if the pending flag is not cleared on time.
If the second NMI among the nested NMI is a Missing-clock NMI, then immediately after MNMIWD reset, there will be another NMI because of the MCLKSTS bit being set.
User NMI handler should not depend on the MNMIFLG.NMIINT bit to determine if there is an active NMI pending and should instead check all the individual bits to determine if an NMI is pending.
This is fixed in Revision A silicon.
0
The Cortex-M3 Memory Protection Unit (MPU) is disabled on the F28M35x Revision 0 silicon.
None. This is fixed in Revision A silicon.
0
The Master Subsystem Boot ROM depends on the MNMIFLG.NMIINT bit to determine if there is a pending NMI on the Master Subsystem. However, as mentioned in the advisory titled "Master Subsystem: MNMIFLG.NMIINT Bit Will Not be Set in Some Cases When an NMI is Still Pending", this bit might not be set. Therefore, the Master Boot ROM NMI handler might return while there is an active NMI pending and MNMIWD counter running. This will trigger MNMIWDRST and reset the entire device. The probability of nested NMI happening during boot time is highly unlikely, unless there is a critical issue elsewhere in the device.
None. This is fixed in Revision A silicon.
0
If there is an NMI at power up or immediately after a reset, the master Boot ROM will branch to the NMI handler. Since access to all memories is blocked upon reset, the NMI handler will not be able to acknowledge the NMI, which will cause the MNMIWD counter to eventually overflow and reset the device. If this NMI is a missing clock NMI, there will be another NMI after the MNMIWD reset because the MCLKSTS bit is not cleared by an external (or watchdog) reset. Therefore, if there is a missing clock condition upon power up or immediately after an external reset, then the device will keep resetting over and over again.
None. This is fixed in Revision A silicon.
0
Parallel boot mode does not transfer data into the device in the intended format.
Use Arm production programming solutions for Cortex-M3 programming.
This is fixed in Revision A silicon.
0
The EALLOW protection of the C28x clocking registers prevents reads to these registers (reads return 0x0000) in addition to preventing writes to the registers (expected behavior of EALLOW-protection) when EALLOW is not set.
Prior to reading C28x clocking registers, the application code must first execute the “EALLOW” command.
This is fixed in Revision A silicon.
0
On a Concerto device, if any SW channel, other than Channel 30, is used for data transfer, then there will be no completion interrupt generated on the µDMA interrupt line when data transfer is done.
The user must poll for the STATE field of the DMASTAT register of SW channel, used for data transfer, to get set to “0x9” to detect completion of data transfer.
This is fixed in Revision A silicon.
0
Due to the internal power-up state of the VCU module, it is possible that the first CRC result will be incorrect. This applies to the first result from each of the eight CRC instructions. This condition can only occur after a power-on reset, but will not necessarily occur on every power on. A warm reset will not cause this condition to reappear.
The application can reset the internal VCU CRC logic by performing a CRC calculation of a single byte in the initialization routine. This routine only needs to perform one CRC calculation and can use any of the CRC instructions. At the end of this routine, clear the VCU CRC result register to discard the result. An example is shown below.
_VCUcrc_reset
MOVZ XAR7, #0
VCRC8L_1 *XAR7
VCRCCLR
LRETR
This is fixed in Revision A silicon.
0
When the prefetch/cache is enabled using the RD_INTF_CTRL register, ECC is verified only on the 64-bit slice that is requested by the CPU; the other 64-bit slice of the 128-bit Flash bank data width is not verified for ECC errors, and instead, is just loaded into the cache. This is applicable for both Cortex-M3 and C28x Flash memory modules.
None. This is fixed in Revision A silicon.
0
On the Control Subsystem, when Flash ECC is enabled (C28 ECC_ENABLE[ENABLE] = 0xA), execution of any F021 Flash API functions will generate a "Flash Uncorrectable" error and an NMI. Flash ECC is enabled by default.
Disable C28x Flash ECC before calling F021 Flash API functions by setting C28 ECC_ENABLE[ENABLE] equal to any value other than 0xA. Then, re-enable C28x Flash ECC by setting C28 ECC_ENABLE[ENABLE] equal to 0xA, if desired, after F021 Flash API functions have finished executing.
This is fixed in Revision A silicon.
0
The getTempSlope() and getTempOffset() functions are not available for use on TMX silicon.
None. This is fixed in Revision A silicon.
0
Resetting the EMAC controller by setting Bit 28 of the SRCR2 register does not automatically reset the Ethernet PHY that is connected to the controller via the MII_PHYRST function on the IO pin.
The microcontroller signal or pin connected to the Reset pin on the Ethernet PHY should be configured as a GPIO instead of as an MII_PHYRST peripheral pin; and the GPIO must be toggled before resetting the EMAC controller. Toggling the GPIO pin (HIGH → LOW → HIGH) will reset the PHY, assuming the reset for your PHY is an active-low signal.
This is fixed in Revision A silicon.
0
Clock Control Registers on the C28x memory map are read-protected by EALLOW.
Enable EALLOW before reading the Clock Control Registers on the C28x memory map.
This is fixed in Revision A silicon.
0
HWBIST is not supported on revision 0 devices.
None. This is fixed in Revision A silicon.
0
On Revision 0 silicon, the Control Subsystem (C28x core) cannot access the EPI. Only the Master Subsystem (M3 core) can. Starting with Revision A silicon, the C28x has read and write data access to the EPI peripheral. Note that C28x use of the EPI for program execution is not supported in any silicon revision.
This is fixed in Revision A silicon.