SPRZ357P August 2011 – June 2020 F28M35E20B , F28M35H22C , F28M35H52C , F28M35H52C-Q1 , F28M35M22C , F28M35M52C
Figure 1 provides an example of the Concerto device markings and defines each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 1. Some prototype devices may have markings different from those illustrated. Figure 2 shows an example of the device nomenclature.
Figure 1. Example of Device Markings | PACKAGE MARKING CODE | SILICON REVISION | REVISION ID ADDRESS | REVISION ID(1) | COMMENTS |
|---|---|---|---|---|
| Blank | 0 | Arm®Cortex®-M3: 0x400F E000
C28x: 0x0883 |
0x0000 | Available as an experimental device. |
| Blank | A | Arm Cortex-M3: 0x400F E000
C28x: 0x0883 |
0x0001 | Available as an experimental device. |
| B | B | Arm Cortex-M3: 0x400F E000
C28x: 0x0883 |
0x0001 | Available as an experimental device and as a qualified production device. |
| E | E | Arm Cortex-M3: 0x400F E000
C28x: 0x0883 |
0x0005 | Available as an experimental device and as a qualified production device. |
Figure 2. Example of Device Nomenclature