SPRUJF1C November 2024 – December 2025 AM2612
The AM261x LaunchPad supports two fully independent BoosterPack XL connectors. BoosterPack site #1 (J1/J3, J2/J4) is located in between the OSPI0 Flash and the micro-B USB Connector. BoosterPack site #2 (J5/J7, J6/J8) is located in between the OSPI0 Flash and the Ethernet add-on board connectors. Each GPIO has multiple functions available through the GPIO mux. The signals connected from the SoC to the BoosterPack headers include:
The AM261x LaunchPad is intended to have full compatibility with four Booster Packs, each with differing pinouts.
The modes of the BoosterPack are controlled using select lines with nets BP_MUX_SW_S1 and BP_MUX_SW_S0 as per the schematic. The BoosterPack modes correspond with the following select line combinations:
| BP_MUX_SW_S1 | BP_MUX_SW_S0 | BoosterPack Mode |
|---|---|---|
| 0 | 0 | Standard LaunchPad/BoosterPack |
| 0 | 1 | Servo Motor Control BoosterPacks |
| 1 | 0 | IO-LINK |
| 1 | 1 | C2000 DRVx BoosterPacks |
In the following pinout tables, a blank "Selected Net" cell indicates that the BoosterPack pin has no external muxing and the net indicated in the BoosterPack Net Name is always selected.