SPMU379A April 2026 – July 2026 TPS25751A
| Description | The 'DBfg' Task is used to clear the dead battery flag. This Task does not disable the PP_EXT input switch that can have been enabled during dead battery operation. |
|---|---|
| INPUT DATAX | None |
| OUTPUT DATAX | Byte 1: Standard Task Return Code. See also Table 6-1. |
| Task Completion | The 'DBfg' Task completes after the effects of clearing the Dead Battery Flag are complete. The task is rejected if the PD controller is not in dead battery mode. |
| Side Effects | The Dead Battery Flag causes the PD Controller to take specific actions, so clearing this flag will have side effects. PD Controller 's power input is forced to VBUS until the Dead Battery Flag is cleared, so executing this Task will change PD Controller 's power input. |
| Additional Information | None |
There are several limitations placed on the PD controller while the Dead-Battery Flag is asserted (PowerPathStatus.PowerSource = 10b).