SPMA072 March   2015 TM4C1294KCPDT , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1294NCZAD , TM4C1299KCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C1299NCZAD , TM4C129EKCPDT , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129ENCZAD , TM4C129XKCZAD , TM4C129XKCZAD , TM4C129XNCZAD , TM4C129XNCZAD

 

  1.   Serial to Ethernet Converter for TM4C129x Microcontrollers Using RTOS
    1.     Trademarks
    2. 1 Introduction
    3. 2 Software Description
    4. 3 Set Up and Program enet_s2e Application
      1. 3.1 Set Up enet_s2e Application
      2. 3.2 Software Modification for DK-TM4C129X
      3. 3.3 Program the enet_s2e Application
    5. 4 Demonstration
      1. 4.1 Set Up EK-TM4C1294XL Board and PC
      2. 4.2 Demonstration
    6. 5 Configuration Webserver
      1. 5.1 Access the Configuration Webserver
        1. 5.1.1 Using the Debug Port
        2. 5.1.2 Using the Finder Utility
      2. 5.2 Different Pages Hosted on the Configuration Webserver
        1. 5.2.1 S2E Status Page
        2. 5.2.2 S2E Port 0 and Port 1 Settings Page
        3. 5.2.3 S2E Miscellaneous Settings Page
    7. 6 Flow Control
    8. 7 Additional Hardware
      1. 7.1 Schematic of RS-232 Level Shifter
      2. 7.2 Connections
      3. 7.3 Bill of Materials (BOM)
    9. 8 References

S2E Miscellaneous Settings Page

The Miscellaneous Settings page, shown in Figure 6, is divided into two parts: “IP Address Selection” and “Restore Factory Defaults”.

The IP Address Selection portion of the page allows configuration of the S2E module to automatically obtain an IP address or use a static IP address at start up. If the “DHCP/AutoIP” option is chosen, the S2E module will first attempt to get an IP address from a DHCP server. If a DHCP server cannot be located, the S2E module will obtain a link local IP address using the AutoIP protocol. If the “Static IP” option is chosen, the “Static IP Address”, “Subnet Mask”, and “Default Gateway” fields need to be filled in. Clicking the “Update Settings” button causes the settings to be saved.

The Restore Factory Defaults portion of the page allows restoring all of the options to their factory default states.

fig6_spma072.gifFigure 6. S2E Miscellaneous Settings Page