SLVUDW8 May 2026
Standard commands are common commands from the Smart Battery Specification (SBS) industry-standard which defines smart battery interfacing. Standard commands use a command code pair to associate the registers associated with each command. Address read and write commands to the LSB of the command code.
Example: Read the RelativeStateOfCharge.
Figure 7-1 shows 0x17 00 in the Data column of the Transaction Log sub-window. This value is 23 in decimal, corresponding to the RSOC%.
Figure 7-1 Standard Data Command Example