SLVUDW8 May 2026
This section describes the process of finding the chemistry identifier, sometimes referred to as "Chemical ID" or "ChemID", of a battery that will be used. The ChemID is a necessary element of the Dynamic Z-Track algorithm that needs to be identified before performing a learning cycle. For the Golden File creation process, this battery must be the same type as the battery that will be used in production. Also use this battery for the proceeding sections.
Texas Instruments has a database of thousands of battery profiles, and the ChemID selection process identifies the exact battery profile or the most similar profile. This ChemID is programmed into the gauge, updating dataflash with the battery profile. The IT algorithm uses this profile for capacity learning, resistance learning, capacity prediction, and other features.
The Chemical ID selection process consists of recording the current, voltage, and temperature (IVT) of a battery during a charge and discharge. This data is submitted to the online Gauging Parameter Calculator (GPC) Tool, which gives the customer a report with a best-fit Chemistry ID to program into their gauge. The process performed with this hardware is a charge-relaxation-discharge-relaxation test. A programmable power supply is recommended for this process.