SLVUDW8 May 2026
Convert the .log file to a .csv file by renaming the file format. Create a blank .csv file and copy into the first, second, third, and fourth columns the time, voltage, current, and temperature, respectively. Verify that the units for each column are seconds, millivolts, milliamps, and Celsius. The first row can be names for each of the columns, which the tool skips assuming there is only one row of names before the data begins. Figure 5-4 is an example of the required .csv file formatting as well as the first few rows of data.
Figure 5-4 Cell Formatting for .csvAfter processing, an e-mail with a report that indicates the results of the process of the tool is sent to the e-mail address you provided when logging into ti.com to use the GPC Tool. The report contains the selected ChemID and a list of additional ChemIDs that satisfy the "less than 3%" error criteria. For example, this report can be useful to verify that a ChemID used previously is still suitable. The report shows any formatting mistakes or other errors.