SLVUDQ2 March 2026
The TPS25730AEVM evaluation module can configure the TPS25730A device without the need to program the device or use software. As the TPS25730A device is a USB-PD controller for use in sink-only applications, the following sink capabilities of the TPS25730AEVM evaluation module are configurable:
The TPS25730AEVM evaluation module configures the listed capabilities using the ADCIN1, ADCIN2, ADCIN3, ADCIN4, and PD5VMAX input pins of the TPS25730A device. The TPS25730AEVM evaluation module utilizes four sets of switches. Each set of switches corresponds to one of the four ADCIN pins, and the PD5VMAX pin is configured by a jumper on the TPS25730AEVM EVM.