SLVUCG6 November   2022 TPS650350-Q1

 

  1.   TPS650350-Q1 EVM User's Guide
  2.   Trademarks
  3. Introduction
  4. Requirements
  5. Operation Instructions
    1. 3.1 Configuring the USB to I2C Adapter
    2. 3.2 Regulator Input Supplies and Features
      1. 3.2.1 Buck 1 Input Supply
      2. 3.2.2 Mid-Vin Buck1 Features
      3. 3.2.3 Buck 2/LDO Input Supply
      4. 3.2.4 Buck 3 Input Supply
      5. 3.2.5 Low-Vin Buck2 and Buck3 Features
      6. 3.2.6 Low Noise LDO Features
    3. 3.3 Selecting the Logic Supply Voltage
  6. EVM Configurations
  7. Test Points
    1. 5.1 Voltage Test Points
  8. Graphical User Interface
    1. 6.1 TPS650350-Q1 EVM Debugging
      1. 6.1.1 I2C Communication Port and Adapter Debugging
      2. 6.1.2 Updating MCU Firmware
    2. 6.2 Navigating the GUI
      1. 6.2.1 Home
      2. 6.2.2 Block Diagram
      3. 6.2.3 Registers
      4. 6.2.4 Device Configuration
        1. 6.2.4.1 Using Device Configuration to Define Spin Settings
        2. 6.2.4.2 Configuring the Power Sequence
      5. 6.2.5 Re-Program PMIC
    3. 6.3 In-Circuit Programming
  9. Typical Performance Plots
    1. 7.1 Power Sequence Plots
    2. 7.2 Load Transient Plots
    3. 7.3 Output Voltage Ripple Plots
    4. 7.4 LDO Output Noise
  10. TPS650350-Q1 EVM Schematic
  11. TPS650350-Q1 EVM PCB Layers
  12. 10TPS650350-Q1 EVM Bill of Materials

Updating MCU Firmware

If the EVM on-board MCU is showing up under the Device Manager with a Stellaris... title, the MCU firmware needs to be updated to communicate with the GUI. One way to do this is with TI's free LM Flash Programmer tool. Once the firmware is updated, the MCU is shown as ACCtrl... COM ports in the Device Manager.

  1. Download the GUI source files from the Gallery. The EVM firmware is the .bin file located in the install_image_TPS6503xx-Q1_GUI/TPS6503xx-Q1_GUI/app/firmware folder.
  2. Open LM Flash Programmer with the EVM connected through USB.
  3. Select USB DFU in the Configuration tab. The Stellaris device is shown in the device list box after refreshing.
  4. Select the Program tab.
  5. Browse to the .bin file downloaded from the GUI.
  6. Leave all other settings as default.
  7. Click Program.