SLVUBT1A October   2019  – June 2020 TPS50601A-SP

 

  1.   TPS50601A-SP Worst Case Analysis Unencrypted PSpice Average Model User's Guide
    1.     Trademarks
    2. 1 TPS50601A-SP WCA Model Specification
    3. 2 Default Parameters
    4. 3 Example of using model with Cadence Pspice (17.2.0)
      1. 3.1 Creating a part from the netlist file
      2. 3.2 Steps to create project in Capture
      3. 3.3 Creating the schematic in Capture
    5. 4 Simulating the Model
      1. 4.1 Monte Carlo Analysis of Output Voltage
      2. 4.2 Frequency Response Analysis
        1. 4.2.1 Analyzing Frequency Response with Bode Plot
        2. 4.2.2 Analyzing Frequency Response with Histogram
  2.   Revision History

Creating the schematic in Capture

The following steps explain the procedure for developing a schematic in Capture using the part created from the netlist:

  1. Open PAGE1 under the SCHEMATIC1 folder below the .dsn file.
  2. Page1.png
  3. Select Place → Part to open the Place Part window. Click on the square icon shown in the following image to add libraries to the project.
  4. Setup9.png
  5. Select all default library files of PSPICE from installation directory and click "Open". (Default Location: “C:\Cadence\SPB_17.2\tools\capture\library\pspice”) Note: This step can be omitted if the default libraries have already been added to Capture.
  6. In the Part search window, type “TPS50601A-SP_AVG” and select the model.
  7. Place_Part.png
  8. Double click on the part in the Part List window and place it by left clicking the cursor on the PAGE1 to place the part. Once the part is placed, the symbol can be edited by selecting the part, right clicking, and choosing "Edit Part".
  9. Edit_Part.png
  10. The part can be resized and pins can be moved to more convenient positions by clicking and dragging them.
  11. Part.png
  12. After editing the part, close the tab to save changes. Choose "Update Current" in the pop-up.
  13. Dialog1.png
  14. Multiple controllable parameters are present in the model, which can be varied to analyze the model functionality. The default values for these parameters can be found in Section 2. To enable easy access to these parameters, make them visible by double clicking the part. The following window will then appear:
  15. Parameters.png
  16. Select all the parameters highlighted above and click the "Display" button. In the pop-up, select "Name and Value" and click "OK".
  17. Name_Value.png
  18. Now, the part must be associated with the netlist. Select the part, right click, and choose "Associate Pspice Model".
  19. Associate_Model.png
  20. Two pop-ups will appear to confirm the operation. Click "Yes" for both.
  21. Pop1.png
    Pop2.png
  22. In the Associate Pspice Model dialogue box, choose the netlist file (***.lib), select the model, and click "Update All".
  23. Associate_Model2.png
  24. A pop-up will appear with successful update message. Click "OK".
  25. Pop3.png
  26. Add the remaining components to complete the schematic as shown in Figure 1.
  27. Schematic.pngFigure 1. Model Schematic