SLVUBT1A October   2019  – June 2020 TPS50601A-SP

 

  1.   TPS50601A-SP Worst Case Analysis Unencrypted PSpice Average Model User's Guide
    1.     Trademarks
    2. 1 TPS50601A-SP WCA Model Specification
    3. 2 Default Parameters
    4. 3 Example of using model with Cadence Pspice (17.2.0)
      1. 3.1 Creating a part from the netlist file
      2. 3.2 Steps to create project in Capture
      3. 3.3 Creating the schematic in Capture
    5. 4 Simulating the Model
      1. 4.1 Monte Carlo Analysis of Output Voltage
      2. 4.2 Frequency Response Analysis
        1. 4.2.1 Analyzing Frequency Response with Bode Plot
        2. 4.2.2 Analyzing Frequency Response with Histogram
  2.   Revision History

Creating a part from the netlist file

In order to run a simulation, the netlist file must be used to create a part that can be used in the schematic.

  1. First, open the "Model Editor" Application.
  2. Model_Editor.png
  3. Then select File → Open and choose the netlist file (***.lib).
  4. Once the netlist opens, select File → Export to Part Library...
  5. Export_Part.png
  6. The Create Parts for Library dialogue box will open. Click "OK" to generate the part library in the default location. This will create a ***.olb file with the same name and location as the netlist file.