SLVK268 June   2026 OPA4H838-SEP

 

  1.   1
  2.   2
  3.   Trademarks
  4. 1Introduction
  5. 2Single-Event Effects (SEE)
  6. 3Device and Test Board Information
  7. 4Irradiation Facility and Setup
  8. 5Test Setup and Procedures
  9. 6Destructive Single-Event Effects (DSEE)
    1. 6.1 Single-Event Latch-up (SEL) Results
  10. 7Single-Event Transients (SET)
  11. 8Summary
  12. 9References

Irradiation Facility and Setup

The heavy-ion species used for the SEE studies on this product are provided and delivered by the TAMU Cyclotron Radiation Effects Facility using a superconducting cyclotron and an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, ion beams had good flux stability and high irradiation uniformity over a 1in diameter circular cross-sectional area for the in-air station. Uniformity is achieved by magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude. For the bulk of these studies, ion flux of 105 ions/cm2·s is used to provide heavy-ion fluences of 107 ions/cm2. The TAMU facility uses a beam port that has a 1mil Aramica window to allow in-air testing while maintaining the vacuum within the particle accelerator. The in-air gap between the device and the ion beam port window is maintained at 40mm for all runs.

For these experiments Silver (109Ag), Krypton (84Kr), Copper (63Cu), Argon (40Ar), Neon (20Ne) and Nitrogen (14N) are used. The angle is held to 0°, but different distances between the device and beam are used to increment the LETEFF. Ion beam uniformity for all tests is in the range of 92 to 97%.

Figure 4-1 shows the OPA4H838-SEP device under test (DUT) in the AMP-PDK-EVM used for data collection at the TAMU facility. Although not visible in this photo, the beam port has a 1mil Aramica window to allow in-air testing while maintaining the vacuum within the accelerator with only minor ion energy loss.

OPA4H838-SEP Photograph of the OPA4H838-SEP EVM in Front of the Heavy-Ion Beam Exit Port at the Texas A&M CyclotronFigure 4-1 Photograph of the OPA4H838-SEP EVM in Front of the Heavy-Ion Beam Exit Port at the Texas A&M Cyclotron
OPA4H838-SEP Photograph of the OPA4H838-SEP EVM
                    Thermal Image for SELFigure 4-2 Photograph of the OPA4H838-SEP EVM Thermal Image for SEL