SLVK197 April   2026 SN54SC1G08-SEP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Overview
  5. 2Single-Event Effects (SEE)
  6. 3Test Device and Test Board Information
  7. 4Irradiation Facility and Setup
  8. 5Results
    1. 5.1 Single-Event Latch-up (SEL) Results
    2. 5.2 Single-Event Transients (SET) Results
  9. 6Event Rate Calculations
  10. 7Summary
  11. 8References

Irradiation Facility and Setup

The heavy-ion species used for the SEL studies on this product were provided and delivered by the MSU Cyclotron Radiation Effects Facility using a superconducting cyclotron and an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, ion beams had good flux stability and high irradiation uniformity over a 1in diameter circular cross-sectional area for the in-air station. Uniformity is achieved by magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude. For this study, ion flux of 1 × 105 ions / cm2-s were used to provide heavy-ion fluences of approximately 1 × 107 ions / cm2 for SEL testing. For the experiments conducted on this report, 109Ag ions at angle of incidence of 0° for an LETEFF of 47 MeV × cm2 / mg were used. The total kinetic energy of 109Ag in the vacuum is 2.125GeV (19.5 MeV/nucleon). Ion uniformity for these experiments was 91.54%.

Figure 4-1 shows one of the three SN54SC1G08-SEP test boards used for experiments at the MSU facility. The in-air gap between the device and the ion beam port window was maintained at 50mm for all runs.

The heavy ion species used for the SEL studies on this product were provided and delivered by the Facility for Rare Isotope Beams (FRIB) at Michigan State University (FRIB Single Event Effects (FSEE) Facility’s linear accelerator.) The FSEE Facility has a dedicated beamline built on the FRIB linac infrastructure with a user experimental station at the end of the FSEE beamline. Ion beams are delivered with high uniformity over a 1-inch diameter exposure area using a thin vacuum window. For this study, ion flux of 1 × 105 ions / cm2-s was used to provide heavy ion fluence of 1 × 107 ions / cm2 using 129Xe ion at a linac energy of 25 MeV / µ. Ion beam uniformity for all tests was 96.42%.

Figure 4-2 shows one of the three SN54SC1G08-SEP test boards used for experiments at the MSU facility. The in-air gap between the device and the ion beam port window was maintained at 70mm for all runs.

 SN54SC1G08-SEP Evaluation Board at the MSU Facility (SEL)Figure 4-1 SN54SC1G08-SEP Evaluation Board at the MSU Facility (SEL)
 SN54SC1G08-SEP Thermal Image for SELFigure 4-3 SN54SC1G08-SEP Thermal Image for SEL
 SN54SC1G08-SEP Evaluation Board at the MSU Facility (SET)Figure 4-2 SN54SC1G08-SEP Evaluation Board at the MSU Facility (SET)