SLVK183 February   2025 TPS7H6005-SP , TPS7H6015-SP , TPS7H6025-SP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. Single-Event Effects (SEE)
  6. Device and Test Board Information
  7. Irradiation Facility and Setup
  8. Depth, Range, and LETEFF Calculation
  9. Test Setup and Procedures
  10. Destructive Single-Event Effects (DSEE)
    1. 7.1 Single-Event Latch-up (SEL) Results
    2. 7.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. Single-Event Transients (SET)
  12. Event Rate Calculations
  13. 10Summary
  14.   A References

Single-Event Transients (SET)

The primary focus of SETs were heavy-ion-induced transient upsets on the output signals HO and LO (with a 1nF capacitive load on the outputs as seen in block diagram). SET testing was done at room temperature across two ion species, 109Ag, and 165Ho which produced a range of LETEFF of 48 to 75MeV × cm2 / mg, for more details see Table 8-1. HO and LO were monitored by two different scopes, a NI PXIe-5110 and a MSO58B oscilloscope. During PWM and IIMSW mode testing, each scope was configured to trigger based on an outside pulse width measurement, where the window for the output signal was 20% (±200ns). During the IIMST modes, the same two scopes were used, however, the trigger was a window which was 500mV above or 500mV below 0V with the signals AC-coupled. The signals in this mode were monitored to see if the signal ever went low when the signal needed to have been high, or high when the signal needed to have been low. During all SET testing, there was no cross-conduction in either PWM or IIM mode and in IIM mode the only transient that occurred was a high to low transient, no signals ever turned on when not required. For all recorded transients, there were never cases where the pulse deviated to be greater than 20%. The only captured SETs were missed pulses that lasted for about 5µs and were always self recoverable. During the IIM mode testing with LO high and during the PWM mode testing during a LO transient, the signature of the transient shows that there is some overshoot (worst recorded overshooots were 410mV during static and approximately 480mV during switching) before leveling back out to 5V during the turn on. This is consistent across all transients, but all signals do recover back to nominal after the overshoot in about 50 µs. Because of this BP5L was monitored on the MSO58B to show that this overshoot is from the internal LDO.

Waveform size, sample rate, trigger type, value, and signal for all scopes used is listed in Table 8-1.

Table 8-1 Scope Settings
Scope Model Trigger Signal Trigger Type Trigger Value Record Length Sample Rate
MSO58B LO Pulse Width and Window ± 20% / ±500mV 20μs / div 250MS / s
BP5L N/A N/A
PXIe-5110 HO Pulse Width and Window ± 20% / ±500mV 20k 100MS / s
Table 8-2 Summary of TPS7H60x5-SP SET Test Condition and Results
Run Number Unit Number Variant Ion LETEFF (MeV × cm2 / mg) Flux (ions × cm2 / s) Fluence (ions / cm2) Mode MSO58B LO Number PXIe-5110 HO Number

35

2

TPS7H6005 165Ho 75 6.33 × 104 1 × 107 PWM

2

0

36

4

TPS7H6005 165Ho 75 8.12 × 104 1× 107 IIMENSW

0

0

37

5

TPS7H6005 165Ho 75 7.14 × 104 1 × 107 IIMDISSW

4

4

38

7

TPS7H6005 107Ag

58

6.87 × 104 1 × 107 PWM 0

0

39

7

TPS7H6005 107Ag

58

6.50 × 104 1 × 107 IIMENSW

0

0

40

8

TPS7H6005 107Ag

58

1.13 × 105 1 × 107 IIMDISSW

0

0

41

9

TPS7H6005 107Ag

48

1.09 × 105 1 × 107 PWM

0

0

 HO SET Run 35 (PWM Mode, fsw = 500kHz)Figure 8-1 HO SET Run 35 (PWM Mode, fsw = 500kHz)
 LO SET Run 37 (IIM-Disabled Mode, fsw = 500kHz)Figure 8-2 LO SET Run 37 (IIM-Disabled Mode, fsw = 500kHz)