SLVK183 February   2025 TPS7H6005-SP , TPS7H6015-SP , TPS7H6025-SP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. Single-Event Effects (SEE)
  6. Device and Test Board Information
  7. Irradiation Facility and Setup
  8. Depth, Range, and LETEFF Calculation
  9. Test Setup and Procedures
  10. Destructive Single-Event Effects (DSEE)
    1. 7.1 Single-Event Latch-up (SEL) Results
    2. 7.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. Single-Event Transients (SET)
  12. Event Rate Calculations
  13. 10Summary
  14.   A References

Single-Event Latch-up (SEL) Results

During the SEL testing the device was heated to 125°C by using a Closed-Loop PID controlled heat gun (MISTRAL 6 System (120V, 2400W). The temperature of the die was verified using thermal camera prior to exposure to heavy ions.

The species used for the SEL testing was Homium (165Ho at 15 MeV / nucleon). For the 165Ho ion an angle of incidence of 0° was used to achieve an LETEFF = 75 MeV × cm2 / mg (for more details, see Table 8-4). The kinetic energy in the vacuum for this ions is 2.474 GeV. Flux of approximately 105 ions / cm2× s and a fluence of approximately 107 ions / cm2 per run was used. Run duration to achieve this fluence was approximately two minutes. The four devices were powered up and exposed to the heavy-ions using the maximum recommended input voltage and boot voltage of 14V. The ASW (High-Side Driver Signal Return) was set to 150V with respect to AGND (low-side driver signal return). The device was set in both PWM and IIM modes during testing. For more information see Single-Event Effects section. No SEL events were observed during all nine runs, indicating that the TPS7H60x5-SP is SEL-free up to 75 MeV × cm2 / mg. Table 8-4 shows the SEL test conditions and results. Figure 7-1 shows a plot of the current versus time for run 1.

Table 7-1 Summary of TPS7H60x5-SP SEL Test Condition and Results
Run Number Unit Number Variant Ion LETEFF (MeV × cm2 / mg) Flux (ions × cm2 / s) Fluence (ions / cm2) VIN

(V)

VBOOT

(V)

Mode EN/HI PWM/LI SEL (# Events)
1 1 TPS7H6005 165Ho 75 1.9 × 104 1 × 107 14 14 PWM 14VDC 14Vpk-pk 500kHz 0
2 1 TPS7H6005 165Ho 75 3.63 × 104 1 × 107 14 14 PWM 14VDC 14Vpk-pk 1MHz 0
3 1 TPS7H6005 165Ho 75 1.91 × 104 1 × 107 14 14 PWM 14VDC 14Vpk-pk 2MHz 0
4

3

TPS7H6005 165Ho 75 1.85 × 104 1 × 107 14 14 IIMENST 14VDC 0V 0
5

3

TPS7H6005 165Ho 75 2.29 × 104 1 × 107 14 14 IIMENST 0V 14VDC 0
6 3 TPS7H6005 165Ho 75 2.45 × 104 1 × 107 14 14 IIMENSW 14Vpk-pk 500kHz 14Vpk-pk 500kHz 0
7

5

TPS7H6005 165Ho 75 2.81 × 104 1 × 107 14 14 IIMDISSW 14Vpk-pk 500kHz 14Vpk-pk 500kHz 0
8

5

TPS7H6005 165Ho 75 1.96 × 104 1 × 107 14 14 IIMDISST 14VDC 0V 0
9

5

TPS7H6005 165Ho 75 2.941× 104 1 × 107 14 14 IIMDISST 0V 14VDC 0

10

10

TPS7H6015 165Ho 75 2.95 × 104 1 × 107 14 14 PWM 14VDC 14Vpk-pk 500kHz 0

11

11

TPS7H6015 165Ho 75 5.80 × 104 1 × 107 14 14 IIMENSW 14Vpk-pk 500kHz 14Vpk-pk 500kHz 0

12

12

TPS7H6015 165Ho 75 4.93 × 104 1 × 107 14 14 IIMDISSW 14Vpk-pk 500kHz 14Vpk-pk 500kHz 0

13

13

TPS7H6025 165Ho 75 8.40 × 104 1 × 107 14 14 PWM 14VDC 14Vpk-pk 500kHz 0

14

14

TPS7H6025 165Ho 75 3.20 × 104 1 × 107 14 14 IIMENSW 14Vpk-pk 500kHz 14Vpk-pk 500kHz 0

Using the MFTF method shown in Single-Event Effects (SEE) Confidence Interval Calculations and combining (or summing) the fluences of the four runs at 125°C (9 × 107), the upper-bound cross-section (using a 95% confidence level) is calculated as:

Equation 1. σ S E L   2.63   x   10 - 8   c m 2 / d e v i c e   f o r   L E T E F F   =   75   M e V · c m 2 / m g   a n d   T   =   125 ° C
 SEL Run 1 (PWM Mode,
                        fsw = 500kHz) Figure 7-1 SEL Run 1 (PWM Mode, fsw = 500kHz)
 SEL Run 2 (PWM Mode,
                        fsw = 1MHz) Figure 7-2 SEL Run 2 (PWM Mode, fsw = 1MHz)
 SEL Run 3 (PWM Mode,
                        fsw = 2MHz) Figure 7-3 SEL Run 3 (PWM Mode, fsw = 2MHz)
 SEL Run 4 (IIM Enabled Mode,
                    PWM/LI = 14V) Figure 7-4 SEL Run 4 (IIM Enabled Mode, PWM/LI = 14V)
 SEL Run 9 (IIM Disabled Mode,
                    EN/HI = 14V) Figure 7-5 SEL Run 9 (IIM Disabled Mode, EN/HI = 14V)