SLUUCK2A October   2022  – November 2022

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 EVM Features
    2. 1.2 General Descriptions
  4. 2Testing Procedures
    1. 2.1 Equipment
    2. 2.2 Hardware Setup
    3. 2.3 Software Setup
    4. 2.4 Test Procedure
      1. 2.4.1 Initial Power Up
      2. 2.4.2 I2C Register Communication Verification
      3. 2.4.3 Charger Mode Verification
      4. 2.4.4 Boost Mode Verification
      5. 2.4.5 Helpful Tips
  5. 3PCB Layout Guideline
  6. 4Board Layout, Schematic, and Bill of Materials
    1. 4.1 Board Layout
    2. 4.2 Schematic
    3. 4.3 Bill of Materials
  7. 5Revision History

I2C Register Communication Verification

Use the following steps for communication verification :

  1. In the EVM software, click the button
    • Verify that the GUI reads in the top right corner.
      Note:

      If the device reads verify Section 2.2 and Section 2.4.1 steps have been followed.

  2. In the Field View (see Figure 2-4), make the following changes as necessary:
    • Set
    • Set
    • Set
      • Note that BQ25622 ILIM pin resistor clamps the input current to 1-A unless that pin is disabled using GUID-20221111-SS0I-ZCKT-VML0-RWZDMTPJN61L-low.png.

    • Set
    • Set
    • Set
    • Set
    • Check
    • Uncheck