SLUUCK2A October   2022  – November 2022

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 EVM Features
    2. 1.2 General Descriptions
  4. 2Testing Procedures
    1. 2.1 Equipment
    2. 2.2 Hardware Setup
    3. 2.3 Software Setup
    4. 2.4 Test Procedure
      1. 2.4.1 Initial Power Up
      2. 2.4.2 I2C Register Communication Verification
      3. 2.4.3 Charger Mode Verification
      4. 2.4.4 Boost Mode Verification
      5. 2.4.5 Helpful Tips
  5. 3PCB Layout Guideline
  6. 4Board Layout, Schematic, and Bill of Materials
    1. 4.1 Board Layout
    2. 4.2 Schematic
    3. 4.3 Bill of Materials
  7. 5Revision History

Software Setup

Use the following to set up the EVM testing software:

  1. On the computer connected to the EV2400 interface board, launch Battery Management Studio (BQStudio). Select Charger as seen in Figure 2-2.
    Figure 2-2 BQStudio Device Type Selection Window
  2. Select the appropriate configuration file based on the device from the window shown in Figure 2-3.
    Figure 2-3 BQStudio Charger Selection Window
  3. Choose GUID-55CE4409-5E61-4F3D-BD0C-C592CBA0310E-low.gif, on the window that appears, and the main window of the BQ25620/2 EVM software will appear, as shown in Figure 2-4.

GUID-20221111-SS0I-CPFR-6JFQ-9MXXBHR98XRB-low.pngFigure 2-4 Main Window of BQ25620/2 EVM Software