SLUUC27C June   2019  – July 2022

 

  1.   BQ25611D, BQ25619 (BMS025) Evaluation Module
  2.   Trademarks
  3. 1Introduction
    1. 1.1 EVM Features
    2. 1.2 I/O Descriptions
  4. 2Test Summary
    1. 2.1 Equipment
    2. 2.2 Equipment Setup
    3. 2.3 Software Setup
    4. 2.4 Test Procedure
      1. 2.4.1 Initial Settings
      2. 2.4.2 Communication Verification
      3. 2.4.3 Charger Mode Verification
      4. 2.4.4 Boost Mode Verification
      5. 2.4.5 Evaluation Results
      6. 2.4.6 Helpful Tips
  5. 3PCB Layout Guideline
  6. 4Board Layout, Schematic, and Bill of Materials
    1. 4.1 Board Layout
    2. 4.2 Schematics
    3. 4.3 Bill of Materials
  7. 5Revision History

Equipment Setup

Use the following list to set up the EVM testing equipment:

  1. Review EVM connections in Table 1-2.
  2. Set PS1 for 5-V DC, 2-A current limit and then turn off the supply.
  3. Connect the output of PS1 in series with a current meter to J1 (VBUS and PGND).
  4. Connect a voltage meter across TP12 (VBUS) and TP31 (PGND), or across J1.
  5. Turn on Load #1, set to constant voltage mode, and output to 2.5-V. Disable Load. Connect Load in series with a current meter (multimeter), ground side, to J4 (BAT and PGND) as shown in Figure 2-1.
  6. Connect one voltage meter across TP16 (BAT) and TP30 (PGND), or across J4-3 and J4-1 as shown in Figure 2-1.
  7. Connect one voltage meter across TP17 (SYS) and TP30 (PGND), or across J2-1 and J2-2 as shown in Figure 2-1.
  8. Connect one voltage meter across TP14 (VPB) and TP32 (PGND), or across J3-1 and J3-2 as shown in Figure 2-1.
  9. Connect the EV2300/2400 USB interface board to the computer with a USB cable and from I2C port to J5 with the 4-pin cable. The connections are shown in Figure 2-1.
  10. Install shunts as shown in Table 1-3.
    Figure 2-1 Original Test Setup for BMS025A